<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: FlexBus operation with limited pins mapped?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-operation-with-limited-pins-mapped/m-p/427202#M24676</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeff,&lt;/P&gt;&lt;P&gt;Of course, the FlexBus module support continuous read or write through the 8-bit or 16-bit port to complete a 32-bit data transfer.&lt;/P&gt;&lt;P&gt;In the reference manual, you can learn more information about the data-byte alignment and physical connections.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Sep 2015 07:25:16 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2015-09-09T07:25:16Z</dc:date>
    <item>
      <title>FlexBus operation with limited pins mapped?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-operation-with-limited-pins-mapped/m-p/427199#M24673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am considering using a K60-series processor as a generic test control processor, and am looking to use as much of the configured functionality as possible alongside a parallel [FlexBus] interface. To maximise other functionality, I am looking to restrict the mapped FlexBus pins to FB_AD0 to FB_AD15 [along with control signals and some chip-selects], and will interface this with 8-bit &amp;amp; 16-bit peripherals as needed. This means that the pins which would normally be associated with FB_AD16 to FB_AD31 are mapped to other functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recognise that I'd need to set CSCR[BLS] = 1 to ensure that the data bus is mapped to the lower FB_AD lines.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Key question is whether I will introduce problems by not bringing out at least a 32-bit bus on external pins? For example: in order to read from 8-bit/16-bit devices, I would effectively have to do a 32-bit read. With the upper 16 bits 'not mapped to pins', what appears on these upper bits as they are read in by the FlexBus function? If I needed further I/O [and only needed - in some implementations - to support 8-bit wide peripherals], is there anything stopping from further reducing this external pin mapping to (say) a 12-bit interface [12-bit address/8-bit data]?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Sep 2015 11:08:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-operation-with-limited-pins-mapped/m-p/427199#M24673</guid>
      <dc:creator>jeffbingham</dc:creator>
      <dc:date>2015-09-04T11:08:05Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus operation with limited pins mapped?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-operation-with-limited-pins-mapped/m-p/427200#M24674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Why would you have to do a 32-bit read when Flexbus is configured with 8 or 16 bit bus width (using the FB_CSCRn register)?&amp;nbsp; I have used Flexbus with 16 bit communications and never had to read 32-bit width; there is no requirement for read alignment or size as far as I know; the application simply reads whatever datatype it is programmed to from a location in the Flexbus' address range, and receives a value (, I believe the default is zero if there are unconfigured pins, but I could be incorrect).&amp;nbsp; There is also nothing stopping you from only configuring 12 pins for addressing and 8 bits for data with Flexbus, in fact, that is exactly what is done when the 8-bit width is selected, and the correct 12 pins are configured (by their corresponding PCRs) for Flexbus. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 00:36:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-operation-with-limited-pins-mapped/m-p/427200#M24674</guid>
      <dc:creator>nicholasf</dc:creator>
      <dc:date>2015-09-09T00:36:08Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus operation with limited pins mapped?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-operation-with-limited-pins-mapped/m-p/427201#M24675</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think you are right: I've just been reading through the user manual again and it indicates that a 32-bit read from [for example] an 8-bit register would read four consecutive addresses. I also noted that not all 32 of the FB_AD pins are brought out on all devices [eg: 100-pin LQFP K64 device], which implies that what I am looking to do is already enforced in at least some implementations. I understand that the device still reads into 32-bit registers [so would guess that the unused bits in the register are zeroed]. Thanks for the reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 07:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-operation-with-limited-pins-mapped/m-p/427201#M24675</guid>
      <dc:creator>jeffbingham</dc:creator>
      <dc:date>2015-09-09T07:13:43Z</dc:date>
    </item>
    <item>
      <title>Re: FlexBus operation with limited pins mapped?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-operation-with-limited-pins-mapped/m-p/427202#M24676</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeff,&lt;/P&gt;&lt;P&gt;Of course, the FlexBus module support continuous read or write through the 8-bit or 16-bit port to complete a 32-bit data transfer.&lt;/P&gt;&lt;P&gt;In the reference manual, you can learn more information about the data-byte alignment and physical connections.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 07:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexBus-operation-with-limited-pins-mapped/m-p/427202#M24676</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-09-09T07:25:16Z</dc:date>
    </item>
  </channel>
</rss>