<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Kinetis K64 Ref clock output</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ref-clock-output/m-p/427131#M24666</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can i output a 24MHz clock from the MCU to other IC ? if so, what are the restrictions ?&lt;/P&gt;&lt;P&gt;MK64FN1M0VDC12 is connected to USB HUB, i want to save the cost of 24MHz crystal required by the USB HUB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 01 Oct 2015 07:26:16 GMT</pubDate>
    <dc:creator>eduardrazumovsk</dc:creator>
    <dc:date>2015-10-01T07:26:16Z</dc:date>
    <item>
      <title>Kinetis K64 Ref clock output</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ref-clock-output/m-p/427131#M24666</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can i output a 24MHz clock from the MCU to other IC ? if so, what are the restrictions ?&lt;/P&gt;&lt;P&gt;MK64FN1M0VDC12 is connected to USB HUB, i want to save the cost of 24MHz crystal required by the USB HUB&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Oct 2015 07:26:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ref-clock-output/m-p/427131#M24666</guid>
      <dc:creator>eduardrazumovsk</dc:creator>
      <dc:date>2015-10-01T07:26:16Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 Ref clock output</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ref-clock-output/m-p/427132#M24667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eduard Razumovsky:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It might be possible to use the FTM (FlexTimer) to get a 24 MHz clock. See these similar threads:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/530710"&gt;Re: Unable to get PWM to work with ext crystal-only configuration&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/533105"&gt;Re: What components  do I need to output PWM using FTM module by Processor Expert ?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/358639"&gt;How could I output 50MHz square waveform by using FRDM-K64F?&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BUT, for a USB HUB this would be really not recommended. USB specifications and timings are very strict. So it should be of course better to use an oscillator or crystal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Oct 2015 04:40:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ref-clock-output/m-p/427132#M24667</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-10-07T04:40:29Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis K64 Ref clock output</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ref-clock-output/m-p/427133#M24668</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks a lot Jorge&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Eduard&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Oct 2015 06:14:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-K64-Ref-clock-output/m-p/427133#M24668</guid>
      <dc:creator>eduardrazumovsk</dc:creator>
      <dc:date>2015-10-08T06:14:03Z</dc:date>
    </item>
  </channel>
</rss>