<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックLoad Apps from SD CARD, Execute in RAM</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Load-Apps-from-SD-CARD-Execute-in-RAM/m-p/425717#M24525</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking for someone to either shoot me down or to indicate whether this is plausible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could it be possible to write apps to run on a Cortex-M4 micro? Storing the ELF files on an SD card, reading them into RAM as and when necessary then executing at the entry point. Could these ELF files link to a common library which the main application on the Cortex-M4 uses (almost like a common API for the platform) as well as any ELF files on the SD card?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It all seems pretty feasible but I'm probably missing something huge.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kev&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Jul 2015 13:01:27 GMT</pubDate>
    <dc:creator>weblar</dc:creator>
    <dc:date>2015-07-20T13:01:27Z</dc:date>
    <item>
      <title>Load Apps from SD CARD, Execute in RAM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Load-Apps-from-SD-CARD-Execute-in-RAM/m-p/425717#M24525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm looking for someone to either shoot me down or to indicate whether this is plausible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could it be possible to write apps to run on a Cortex-M4 micro? Storing the ELF files on an SD card, reading them into RAM as and when necessary then executing at the entry point. Could these ELF files link to a common library which the main application on the Cortex-M4 uses (almost like a common API for the platform) as well as any ELF files on the SD card?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It all seems pretty feasible but I'm probably missing something huge.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kev&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2015 13:01:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Load-Apps-from-SD-CARD-Execute-in-RAM/m-p/425717#M24525</guid>
      <dc:creator>weblar</dc:creator>
      <dc:date>2015-07-20T13:01:27Z</dc:date>
    </item>
    <item>
      <title>Re: Load Apps from SD CARD, Execute in RAM</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Load-Apps-from-SD-CARD-Execute-in-RAM/m-p/425718#M24526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello weblar:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since you posted in this space I guess you are referring to a Kinetis MCU with Cortex-M4 core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess your idea is achievable but I am not aware of such implementation. The closest project I know about is uCLinux in K70 platform by third party emcraft. The details are in their page:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.emcraft.com/index.php/products/95" title="http://www.emcraft.com/index.php/products/95"&gt;Linux BSP for Freescale TWR-K70F120M&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry if my response is not concise, that is not a typical use case of Kinetis MCUs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 22:44:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Load-Apps-from-SD-CARD-Execute-in-RAM/m-p/425718#M24526</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-07-29T22:44:33Z</dc:date>
    </item>
  </channel>
</rss>