<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Setting up I2C connections on K70</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424741#M24443</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, it doesn't look like anybody with THAT info is going to respond on THIS thread.&amp;nbsp; I suggest you submit a new question with that specific request.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Apr 2015 10:25:50 GMT</pubDate>
    <dc:creator>egoodii</dc:creator>
    <dc:date>2015-04-22T10:25:50Z</dc:date>
    <item>
      <title>Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424733#M24435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking for some tips and guidance. I am looking to setup an I2C connection between a K70 board and an old TWR-RF board. Can someone direct me to a useful demo or discussion regarding this task? Also I want to make sure I have my jumpers in the proper positions.&lt;/P&gt;&lt;P&gt;For the TWR-RF board I have J8 on and J9 off to manage off board power, a jumper on pins 11 - 12 and 13 - 14 on J1 to manage the I2C data and clock running between the RF board and the elevator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help will be greatly appreciated! Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 13:11:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424733#M24435</guid>
      <dc:creator>nicholasconstan</dc:creator>
      <dc:date>2015-04-20T13:11:09Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424734#M24436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What are your GOALS for the I2C firmware tasks?&amp;nbsp; Are you looking for the 'simplest bare-metal polled interface', or are you looking for a full background, interrupt-driven state machine to handle it all with minimal processor clocks?&amp;nbsp; Or MQX? OR uTasker!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 13:19:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424734#M24436</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2015-04-20T13:19:13Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424735#M24437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My goals are to have a interrupt driven task using MQX. The end result is to have to TWR-LCD screens communicating state changes to one another using zigbee.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 13:39:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424735#M24437</guid>
      <dc:creator>nicholasconstan</dc:creator>
      <dc:date>2015-04-20T13:39:12Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424736#M24438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;More Background information:&lt;/P&gt;&lt;P&gt;The application I am building should result in the ability for two towers to play tic tac toe against one another. The users of the towers can interact with the game using a gui displayed on the TWR-Graphical-LCD. The two towers should then transmit the latest move over a zigbee connection. My thought is that in order to have the zigbee board attached to the TWR-RF communicate to the K70 board I should utilize the I2C connection available through the elevator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I have accomplished thus far is a working tic tac toe gui which stores the games data in an array. I also have a working zigbee connection between two towers. The massive hole is connecting these two working parts together.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 13:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424736#M24438</guid>
      <dc:creator>nicholasconstan</dc:creator>
      <dc:date>2015-04-20T13:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424737#M24439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is this all already running under MQX?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 14:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424737#M24439</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2015-04-20T14:25:22Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424738#M24440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Yes&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 14:26:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424738#M24440</guid>
      <dc:creator>nicholasconstan</dc:creator>
      <dc:date>2015-04-20T14:26:54Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424739#M24441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So I take it you are looking for a 'worked example' of of a proper blocking-task utilizing the MQX I2C interrupt-mode interface.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 18:39:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424739#M24441</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2015-04-20T18:39:50Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424740#M24442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 21:22:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424740#M24442</guid>
      <dc:creator>nicholasconstan</dc:creator>
      <dc:date>2015-04-20T21:22:27Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424741#M24443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Well, it doesn't look like anybody with THAT info is going to respond on THIS thread.&amp;nbsp; I suggest you submit a new question with that specific request.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Apr 2015 10:25:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424741#M24443</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2015-04-22T10:25:50Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up I2C connections on K70</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424742#M24444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nicholas,&lt;/P&gt;&lt;P&gt;as free inspiration you can use my example code for I2C communication with accelerometer sensor:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2023" data-containertype="14" data-objectid="104587" data-objecttype="102" href="https://community.freescale.com/docs/DOC-104587"&gt;https://community.freescale.com/docs/DOC-104587&lt;/A&gt;&lt;/P&gt;&lt;P&gt;It is not what you really want, but it could be better than nothing.&lt;/P&gt;&lt;P&gt;Example used I2C bus in pooling mode and it integrates two approaches for waiting for new data:&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;GPIO pin interrupt could be used for signalize when slave has new data&lt;/LI&gt;&lt;LI&gt;Or master could periodically read slaves status.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2015 10:23:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Setting-up-I2C-connections-on-K70/m-p/424742#M24444</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-05-07T10:23:16Z</dc:date>
    </item>
  </channel>
</rss>