<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ADC value when input is less than 0V in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-value-when-input-is-less-than-0V/m-p/424693#M24433</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my design I have an ADC single ended input that may experience a voltage as low as -0.1V with respect to the analog Vss. I need to know what the conversion result will be in this case.&lt;/P&gt;&lt;P&gt;Is it 0?&lt;/P&gt;&lt;P&gt;Is it undefined?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jun 2015 14:49:11 GMT</pubDate>
    <dc:creator>williamely</dc:creator>
    <dc:date>2015-06-03T14:49:11Z</dc:date>
    <item>
      <title>ADC value when input is less than 0V</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-value-when-input-is-less-than-0V/m-p/424693#M24433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my design I have an ADC single ended input that may experience a voltage as low as -0.1V with respect to the analog Vss. I need to know what the conversion result will be in this case.&lt;/P&gt;&lt;P&gt;Is it 0?&lt;/P&gt;&lt;P&gt;Is it undefined?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2015 14:49:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-value-when-input-is-less-than-0V/m-p/424693#M24433</guid>
      <dc:creator>williamely</dc:creator>
      <dc:date>2015-06-03T14:49:11Z</dc:date>
    </item>
    <item>
      <title>Re: ADC value when input is less than 0V</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-value-when-input-is-less-than-0V/m-p/424694#M24434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi William Ely,&lt;/P&gt;&lt;P&gt;It will read 0 when -0.1V connect the input pin if VSS is 0V, however I'd highly recommend that the range of the analog input voltage should within Vrefl~Vrefh.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 03:33:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/ADC-value-when-input-is-less-than-0V/m-p/424694#M24434</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-06-04T03:33:20Z</dc:date>
    </item>
  </channel>
</rss>