<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Stock firmware for the TWR-K21D50M</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Stock-firmware-for-the-TWR-K21D50M/m-p/424151#M24376</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where do I find the firmware that comes with this board? I'm asking for the S19 or srec or anything of the like so I can undo any of the changes when I start using the cyclone max.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Sep 2015 14:05:28 GMT</pubDate>
    <dc:creator>jorgesierra</dc:creator>
    <dc:date>2015-09-03T14:05:28Z</dc:date>
    <item>
      <title>Stock firmware for the TWR-K21D50M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Stock-firmware-for-the-TWR-K21D50M/m-p/424151#M24376</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Where do I find the firmware that comes with this board? I'm asking for the S19 or srec or anything of the like so I can undo any of the changes when I start using the cyclone max.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 14:05:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Stock-firmware-for-the-TWR-K21D50M/m-p/424151#M24376</guid>
      <dc:creator>jorgesierra</dc:creator>
      <dc:date>2015-09-03T14:05:28Z</dc:date>
    </item>
    <item>
      <title>Re: Stock firmware for the TWR-K21D50M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Stock-firmware-for-the-TWR-K21D50M/m-p/424152#M24377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can get from here &lt;A href="http://www.freescale.com/webapp/sps/download/license.jsp?colCode=TWR-K21D50M_SC_LAB&amp;amp;location=null&amp;amp;Parent_nodeId=1343143755544690978100&amp;amp;Parent_pageType=product" title="http://www.freescale.com/webapp/sps/download/license.jsp?colCode=TWR-K21D50M_SC_LAB&amp;amp;location=null&amp;amp;Parent_nodeId=1343143755544690978100&amp;amp;Parent_pageType=product"&gt;TWR-K21D50M Sample Code &lt;/A&gt;the sample code for the board, inside the folder that is installed in the next path TWR-K21D50M Sample Code\TWR-K21D50M_SC\build\cw\TWR-K21D50M-OOBE you can find the Out of the Box demo for the board, this is the source code for the demo, you can find the version for IAR IDE also.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this information can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 20:35:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Stock-firmware-for-the-TWR-K21D50M/m-p/424152#M24377</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2015-09-03T20:35:48Z</dc:date>
    </item>
    <item>
      <title>Re: Stock firmware for the TWR-K21D50M</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Stock-firmware-for-the-TWR-K21D50M/m-p/424153#M24378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks. In the future, where would I have found this if I didn't have this forum to save my life?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 19:13:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Stock-firmware-for-the-TWR-K21D50M/m-p/424153#M24378</guid>
      <dc:creator>jorgesierra</dc:creator>
      <dc:date>2015-09-08T19:13:13Z</dc:date>
    </item>
  </channel>
</rss>