<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 How to use i2c on the FRDM-KE02Z</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-i2c-on-the-FRDM-KE02Z/m-p/423946#M24353</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am doing a project with the FRDM-KE02Z board. I need to use i2c, which I am new to. The SDA and SCL pins are being used by an accelerometer&amp;nbsp; which i have no plan to use. How do I gain access to the pins without using the accelerometer? I know that you can use many devices on on i2c "line", other than that I am very new to this communication type. Any information would be extremely useful.&lt;/P&gt;&lt;P&gt;Dan Bean&lt;/P&gt;&lt;P&gt;Intern&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Jun 2015 14:14:32 GMT</pubDate>
    <dc:creator>danbean</dc:creator>
    <dc:date>2015-06-03T14:14:32Z</dc:date>
    <item>
      <title>How to use i2c on the FRDM-KE02Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-i2c-on-the-FRDM-KE02Z/m-p/423946#M24353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am doing a project with the FRDM-KE02Z board. I need to use i2c, which I am new to. The SDA and SCL pins are being used by an accelerometer&amp;nbsp; which i have no plan to use. How do I gain access to the pins without using the accelerometer? I know that you can use many devices on on i2c "line", other than that I am very new to this communication type. Any information would be extremely useful.&lt;/P&gt;&lt;P&gt;Dan Bean&lt;/P&gt;&lt;P&gt;Intern&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jun 2015 14:14:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-i2c-on-the-FRDM-KE02Z/m-p/423946#M24353</guid>
      <dc:creator>danbean</dc:creator>
      <dc:date>2015-06-03T14:14:32Z</dc:date>
    </item>
    <item>
      <title>Re: How to use i2c on the FRDM-KE02Z</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-i2c-on-the-FRDM-KE02Z/m-p/423947#M24354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;SPAN class="j-post-author"&gt;you just need to define your slave address different from the on-board acelerometer adress. &lt;/SPAN&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to here :&lt;A href="https://community.nxp.com/message/516347"&gt;Re: How to access PTA2 and PTA3 pins for I2C communication on FRDM-KE02Z board?&lt;/A&gt;&lt;/P&gt;&lt;P&gt;You are the same problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If still have any question , please contact us!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alice&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jul 2015 02:22:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-use-i2c-on-the-FRDM-KE02Z/m-p/423947#M24354</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2015-07-03T02:22:11Z</dc:date>
    </item>
  </channel>
</rss>