<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK02 DAC output logic level during Power-On Reset (POR)</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-DAC-output-logic-level-during-Power-On-Reset-POR/m-p/422615#M24242</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Madam,&lt;/P&gt;&lt;P&gt;I'm using the K02FN64VFM10, and would like to use the DAC port to generate a slope signal. Processor Expert is used to initialize the DAC module.&lt;/P&gt;&lt;P&gt;During the power-on process, the DAC output stays at 3 V for about 250 ms, and then drops to 0 V and start to generate the slope signal. &lt;/P&gt;&lt;P&gt;As in the figure below, the yellow line is the DAC output, which stays high during the first 250 ms. The green line is the 3.3 V VDD signal (Power supply) and the pink line is a GPIO output, which generate a high level output immediately after the automatic initialization by Processor Expert.@@&lt;/P&gt;&lt;P&gt;I'm wondering if the DAC output logic level could be programmed to 0 V during reset at the very beginning.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58127iA52EAC710BF7883A/image-size/large?v=v2&amp;amp;px=999" title="IMG_1212.JPG" alt="IMG_1212.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for any kind of help!&lt;/P&gt;&lt;P&gt;Marie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Sep 2015 03:10:31 GMT</pubDate>
    <dc:creator>marielu</dc:creator>
    <dc:date>2015-09-30T03:10:31Z</dc:date>
    <item>
      <title>K02 DAC output logic level during Power-On Reset (POR)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-DAC-output-logic-level-during-Power-On-Reset-POR/m-p/422615#M24242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sir or Madam,&lt;/P&gt;&lt;P&gt;I'm using the K02FN64VFM10, and would like to use the DAC port to generate a slope signal. Processor Expert is used to initialize the DAC module.&lt;/P&gt;&lt;P&gt;During the power-on process, the DAC output stays at 3 V for about 250 ms, and then drops to 0 V and start to generate the slope signal. &lt;/P&gt;&lt;P&gt;As in the figure below, the yellow line is the DAC output, which stays high during the first 250 ms. The green line is the 3.3 V VDD signal (Power supply) and the pink line is a GPIO output, which generate a high level output immediately after the automatic initialization by Processor Expert.@@&lt;/P&gt;&lt;P&gt;I'm wondering if the DAC output logic level could be programmed to 0 V during reset at the very beginning.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58127iA52EAC710BF7883A/image-size/large?v=v2&amp;amp;px=999" title="IMG_1212.JPG" alt="IMG_1212.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance for any kind of help!&lt;/P&gt;&lt;P&gt;Marie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Sep 2015 03:10:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-DAC-output-logic-level-during-Power-On-Reset-POR/m-p/422615#M24242</guid>
      <dc:creator>marielu</dc:creator>
      <dc:date>2015-09-30T03:10:31Z</dc:date>
    </item>
    <item>
      <title>Re: K02 DAC output logic level during Power-On Reset (POR)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-DAC-output-logic-level-during-Power-On-Reset-POR/m-p/422616#M24243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello marie lu:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried with a FRDM-K22 and I do not see this behavior. This is what I get (Power ON and then I write random values to DAC):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58632iAE57D47B1FFA5670/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you attach your project?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In particular I want to check the next points:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- What IDE (KDS, IAR, Keil)?&lt;/P&gt;&lt;P&gt;- Processor Expert with or without KSDK?&lt;/P&gt;&lt;P&gt;- Using other components?&lt;/P&gt;&lt;P&gt;- Is auto initialization enabled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 01:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-DAC-output-logic-level-during-Power-On-Reset-POR/m-p/422616#M24243</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-10-05T01:21:10Z</dc:date>
    </item>
    <item>
      <title>Re: K02 DAC output logic level during Power-On Reset (POR)</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-DAC-output-logic-level-during-Power-On-Reset-POR/m-p/422617#M24244</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jorge,&lt;/P&gt;&lt;P&gt;Thank you so much for helping me working on this. &lt;/P&gt;&lt;P&gt;I'm using KDS 3.0.0, Processor Expert with KSDK 1.2.0. Under the projects, I also use ADC, FTM and GPIO modules, with auto initialization enabled. For emulator, I use PE micro multilink universal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on a DC-DC power supply, and the figure I showed you is captured when the power stage is working. When the power stage is not working and only the processor operates, I get the same waveform as yours.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to draw your attention to some details. In your figure, there is a small spike before DAC starts to output, which is highlighted in red circle in the pic below.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58701iAB03C80B2DFBB200/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On my processor, I could also see this spike, but with higher amplitude, as shown below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58808i4BF14CB15EF0A674/image-size/large?v=v2&amp;amp;px=999" title="IMG_1288.JPG" alt="IMG_1288.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I zoom in the spike, and it shows as an increasing slope, and then drops down to zero.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58829i3F043F81F200DEAF/image-size/large?v=v2&amp;amp;px=999" title="IMG_1289.JPG" alt="IMG_1289.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The bandwidth of the scope in the figures above is 200 MHz. Since you also have the spike on your waveform, I assume it's not my measurement problem. I'm wondering what causes this voltage spike, and if there's any method to avoid it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and best wishes,&lt;/P&gt;&lt;P&gt;Marie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Oct 2015 16:48:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-DAC-output-logic-level-during-Power-On-Reset-POR/m-p/422617#M24244</guid>
      <dc:creator>marielu</dc:creator>
      <dc:date>2015-10-05T16:48:31Z</dc:date>
    </item>
  </channel>
</rss>