<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K64 Factory Programmed Firmware in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Factory-Programmed-Firmware/m-p/422270#M24203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are currently developing using a TWR-K64F-120M Tower Module with a view to use a K64 processor in our own board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you confirm what firmware, if any, is pre-programmed into the device from the factory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Kinetis Bootloader Manual it states the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;All future Kinetis devices will arrive with a ROM containing the Kinetis bootloader, while others will arrive pre-programmed from the factory with a one-time-use serial flashloader.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reading the forum and applications notes, however, do not mention that this is the case. Calcification would be much appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jun 2015 09:10:06 GMT</pubDate>
    <dc:creator>ramstell</dc:creator>
    <dc:date>2015-06-23T09:10:06Z</dc:date>
    <item>
      <title>K64 Factory Programmed Firmware</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Factory-Programmed-Firmware/m-p/422270#M24203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are currently developing using a TWR-K64F-120M Tower Module with a view to use a K64 processor in our own board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you confirm what firmware, if any, is pre-programmed into the device from the factory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Kinetis Bootloader Manual it states the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;All future Kinetis devices will arrive with a ROM containing the Kinetis bootloader, while others will arrive pre-programmed from the factory with a one-time-use serial flashloader.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Reading the forum and applications notes, however, do not mention that this is the case. Calcification would be much appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2015 09:10:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Factory-Programmed-Firmware/m-p/422270#M24203</guid>
      <dc:creator>ramstell</dc:creator>
      <dc:date>2015-06-23T09:10:06Z</dc:date>
    </item>
    <item>
      <title>Re: K64 Factory Programmed Firmware</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Factory-Programmed-Firmware/m-p/422271#M24204</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Roger Amstell:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K64 does not have the flashloader integrated from factory. Please check the table in next product page for the supported devices in each category (flash-resident bootloader/flashloader/ROM bootloader):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KBOOT&amp;amp;tid=vanKBOOT" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=KBOOT&amp;amp;tid=vanKBOOT"&gt;Kinetis Bootloader|Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the same link you can download the bootloader firmware to use it with the K64.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this clarifies.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards!,&lt;BR /&gt;Jorge Gonzalez&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jun 2015 16:34:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64-Factory-Programmed-Firmware/m-p/422271#M24204</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-06-23T16:34:03Z</dc:date>
    </item>
  </channel>
</rss>