<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MK21 XTAL32 and Dryice questions</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421050#M24111</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.In fact, I had tested to connect external signal generator 32.768KHz clock to EXTAL32 and XTAL32 separately. The RTC module could work as expected. &lt;/P&gt;&lt;P&gt;While, for the EXTAL32 pin is input, we suggest customer to connect external clock source to EXTAL32 pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. That's right.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Jun 2015 00:02:59 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-06-08T00:02:59Z</dc:date>
    <item>
      <title>MK21 XTAL32 and Dryice questions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421046#M24107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;I have 2 questions:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;1. Is it possible to replace the 32KHz crystal with a MEMS crystal oscillator for the XTAL32 input for the RTC on this device?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d;"&gt;2. Does the dryice require the XTAL32 clock to run if we just want the 32bytes of battery ram? &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2015 22:24:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421046#M24107</guid>
      <dc:creator>PHXFAE</dc:creator>
      <dc:date>2015-06-02T22:24:54Z</dc:date>
    </item>
    <item>
      <title>Re: MK21 XTAL32 and Dryice questions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421047#M24108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alex,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.&amp;nbsp;&amp;nbsp; I think a MEMS crystal oscillator as a external 32KHz clock source (oscillator) should works with RTC module.&lt;/P&gt;&lt;P&gt;I do a test with TWR-K40X256 board, using external signal generator output 32KHz clock as RTC reference clock input to EXTAL32 pin, and the RTC module works as expected.&lt;/P&gt;&lt;P&gt;2. The DryICE module clock source from RTC clock source, which still need external 32KHz clock when do any operation with DryICE module.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 01:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421047#M24108</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-06-04T01:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: MK21 XTAL32 and Dryice questions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421048#M24109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.&amp;nbsp; Just to be clear, you connected the signal generator to the XTAL32 pin correct, not the EXTAL32 pin?&amp;nbsp; Can you please tell me the signal level you used and the VCC you were using for the K40 board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. You are saying that the RTC clock MUST be used when doing anything with DryICE, correct? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx for the help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2015 17:56:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421048#M24109</guid>
      <dc:creator>PHXFAE</dc:creator>
      <dc:date>2015-06-05T17:56:10Z</dc:date>
    </item>
    <item>
      <title>Re: MK21 XTAL32 and Dryice questions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421049#M24110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm sorry. but I change the names around on number 1 above.&amp;nbsp; The question should read -.Just to be clear, you connected the signal generator to the EXTAL32 pin correct, not the XTAL32 pin?&amp;nbsp; Can you please tell me the signal level you used and the VCC you were using for the K40 board?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2015 17:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421049#M24110</guid>
      <dc:creator>PHXFAE</dc:creator>
      <dc:date>2015-06-05T17:58:56Z</dc:date>
    </item>
    <item>
      <title>Re: MK21 XTAL32 and Dryice questions</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421050#M24111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.In fact, I had tested to connect external signal generator 32.768KHz clock to EXTAL32 and XTAL32 separately. The RTC module could work as expected. &lt;/P&gt;&lt;P&gt;While, for the EXTAL32 pin is input, we suggest customer to connect external clock source to EXTAL32 pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. That's right.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Jun 2015 00:02:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK21-XTAL32-and-Dryice-questions/m-p/421050#M24111</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-06-08T00:02:59Z</dc:date>
    </item>
  </channel>
</rss>