<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419424#M23959</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi Ping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks. But I observed that if i write simple c code like&lt;/P&gt;&lt;P&gt;void main()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt; int a, b, c, d, e;&lt;/P&gt;&lt;P&gt;while(1)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; a=3;&lt;/P&gt;&lt;P&gt;&amp;nbsp; b= 3;&lt;/P&gt;&lt;P&gt;&amp;nbsp; c=a+b;&lt;/P&gt;&lt;P&gt;&amp;nbsp; d=a+c;&lt;/P&gt;&lt;P&gt;&amp;nbsp; e= a+c+d;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can put breakpoint in all lines and there is no limit of only 2 breakpoint in the code. How it works?&lt;/P&gt;&lt;P&gt;If there is only 2 breakpoint limitation, it should also not work.&lt;/P&gt;&lt;P&gt;you can try it at your end as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What about software breakpoint?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Aug 2015 10:15:38 GMT</pubDate>
    <dc:creator>gagan</dc:creator>
    <dc:date>2015-08-10T10:15:38Z</dc:date>
    <item>
      <title>Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419422#M23957</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, We are using MKE04z128 micro-controller with IAR compiler and jlink plus programmer. During debugging, if we set more than 2 breakpoint in our code, our application stops working and displays error message "Timeout during programming sector, core does stop and my application hangs and i need to reload the code into the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I know that there is only two hardware breakpoint but microcontroller should allow software breakpoint during debugging.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 11:28:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419422#M23957</guid>
      <dc:creator>gagan</dc:creator>
      <dc:date>2015-08-06T11:28:56Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419423#M23958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gagan,&lt;/P&gt;&lt;P&gt;Debug the KE04 with the Jlink only allow to put 2 breakpoints.&lt;/P&gt;&lt;P&gt;And I've also confirmed it, when I put 3 breakpoints in the demo, an error message would jump out (Fig 1)&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55256i54B42E01A7DD8983/image-size/large?v=v2&amp;amp;px=999" title="2015-08-07_10-03-58.jpg" alt="2015-08-07_10-03-58.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2015 02:17:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419423#M23958</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-08-07T02:17:17Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419424#M23959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hi Ping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks. But I observed that if i write simple c code like&lt;/P&gt;&lt;P&gt;void main()&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt; int a, b, c, d, e;&lt;/P&gt;&lt;P&gt;while(1)&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp; a=3;&lt;/P&gt;&lt;P&gt;&amp;nbsp; b= 3;&lt;/P&gt;&lt;P&gt;&amp;nbsp; c=a+b;&lt;/P&gt;&lt;P&gt;&amp;nbsp; d=a+c;&lt;/P&gt;&lt;P&gt;&amp;nbsp; e= a+c+d;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can put breakpoint in all lines and there is no limit of only 2 breakpoint in the code. How it works?&lt;/P&gt;&lt;P&gt;If there is only 2 breakpoint limitation, it should also not work.&lt;/P&gt;&lt;P&gt;you can try it at your end as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What about software breakpoint?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 10:15:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419424#M23959</guid>
      <dc:creator>gagan</dc:creator>
      <dc:date>2015-08-10T10:15:38Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419425#M23960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gagan,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;And I've run the code you shared, however the breakpoint still is not able to be set if I had already set two and some messages listed below as the Fig 1 illustrates.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52407iC32DCADA325870D0/image-size/large?v=v2&amp;amp;px=999" title="2015-08-11_10-46-53.jpg" alt="2015-08-11_10-46-53.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Fig 1&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 02:54:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419425#M23960</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-08-11T02:54:58Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419426#M23961</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using Jlink Plus which is allowing me to put more than 2 breakpoint and see my below workspace.&lt;/P&gt;&lt;P&gt;Jlink Base allows you to use only two breakpoint.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53280i92EB1F8F7F0D048F/image-size/large?v=v2&amp;amp;px=999" title="breakpoint.png" alt="breakpoint.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In the above workspace, I can set as many breakpoint as required.&lt;/P&gt;&lt;P&gt;However if i tried the same with my code, debugger stops and gives me error message which I mentioned in my original post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am wondering what could be the difference between my code and the above test code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Gagan Gupta&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 04:23:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419426#M23961</guid>
      <dc:creator>gagan</dc:creator>
      <dc:date>2015-08-11T04:23:58Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419427#M23962</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Gagan,&lt;/P&gt;&lt;P&gt;There are two types of breakpoint, one is hardware &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;breakpoint&lt;/STRONG&gt;&lt;/SPAN&gt; which has limitation in number , the other is software breakpoint.&lt;/P&gt;&lt;P&gt;J-Link PLUS support unlimited breakpoint in the flash memory which belongs to the software breakpoint.&lt;/P&gt;&lt;P&gt;So you can set more than 2 breakpoint in the code above, however failed to set in this sort of code which operates some hardware units inside MCU.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 06:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419427#M23962</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-08-11T06:51:55Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419428#M23963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regarding the below point,&lt;/P&gt;&lt;P&gt;"So you can set more than 2 breakpoint in the code above, however failed to set in this sort of code which operates some hardware units inside MCU."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do not agree with it otherwise it defeats the purpse of software breakpoints.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 08:52:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419428#M23963</guid>
      <dc:creator>gagan</dc:creator>
      <dc:date>2015-08-11T08:52:20Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419429#M23964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Software breakpoints will not work on code in flash memory. Software breakpoints work by replacing code in memory with a breakpoint command. To insert the breakpoint in flash memory,&amp;nbsp; you would have to erase an entire sector and rewrite it with the breakpoint command in place. To erase the breakpoint you would need to once again erase the entire sector and replace the code that was originally there.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the reason hardware breakpoints exist. If you could easily replace the opcodes in memory, hardware breakpoints wouldn't be needed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2015 16:49:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419429#M23964</guid>
      <dc:creator>ndavies</dc:creator>
      <dc:date>2015-08-11T16:49:28Z</dc:date>
    </item>
    <item>
      <title>Re: Problem in more than 2 breakpoint use for MKE04Z128 series micro-controller.</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419430#M23965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Try to debug your code in RAM if you want unlimited breakpoint.&lt;/P&gt;&lt;P&gt;If the resource of MCU breakpoint unit has been occupied by hardware breakpoints, then you won't be able to set any software breakpoint. maybe this is the reason why the test code can work with more breakpoints but your code can't.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Aug 2015 01:16:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Problem-in-more-than-2-breakpoint-use-for-MKE04Z128-series-micro/m-p/419430#M23965</guid>
      <dc:creator>jay_heng</dc:creator>
      <dc:date>2015-08-12T01:16:49Z</dc:date>
    </item>
  </channel>
</rss>