<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SPI DMA in SLAVE MODE in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418590#M23848</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremyzhou, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got it right. :smileyhappy: I enabled another DMA channel for transmission. Now DMA0 handles SPI reception and DMA1 handles SPI transmission.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Varun R&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 12 May 2015 09:17:22 GMT</pubDate>
    <dc:creator>varunrajarangan</dc:creator>
    <dc:date>2015-05-12T09:17:22Z</dc:date>
    <item>
      <title>SPI DMA in SLAVE MODE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418586#M23844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to establish full duplex communication through SPI using DMA. So far I am able to receive data from master in blocks(256 bytes). But I am a bit confused in transmitting data back to master. Do I have to enable another channel for transmitting data? or Do I have to enable SPI interrupt? I am using KL05Z.&lt;/P&gt;&lt;P&gt;Please help me guys...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Varun R&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 May 2015 10:28:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418586#M23844</guid>
      <dc:creator>varunrajarangan</dc:creator>
      <dc:date>2015-05-11T10:28:45Z</dc:date>
    </item>
    <item>
      <title>Re: SPI DMA in SLAVE MODE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418587#M23845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Varun，&lt;/P&gt;&lt;P&gt;You needn't wrong it at all. SPI supports full duplex communication and device can transmit and receive data simultaneously when it works in Master mode or Slave mode after you establish the connection likes the Fig 1.&lt;/P&gt;&lt;P&gt;Hope it helps.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22086i80BC402979538BE8/image-size/large?v=v2&amp;amp;px=999" title="2015-05-12_10-45-46.jpg" alt="2015-05-12_10-45-46.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Fig 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 02:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418587#M23845</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-05-12T02:59:31Z</dc:date>
    </item>
    <item>
      <title>Re: SPI DMA in SLAVE MODE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418588#M23846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremyzhou, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My application is in slave mode. I am using DMA to receive data blocks. But how do I put data in the SPI0_D register when working in DMA mode??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Varun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 05:04:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418588#M23846</guid>
      <dc:creator>varunrajarangan</dc:creator>
      <dc:date>2015-05-12T05:04:53Z</dc:date>
    </item>
    <item>
      <title>Re: SPI DMA in SLAVE MODE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418589#M23847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Varun，&lt;/P&gt;&lt;P&gt;The SPI module in KL05 supports both transmit and receive by DMA and about the detail configuration of the DMA integrate with SPI,&lt;/P&gt;&lt;P&gt;I'd highly recommend you should review the chapter 22&amp;nbsp; DMAMUX and chapter 23 DMA Controller Module in the reference manual.&lt;/P&gt;&lt;P&gt;After that, I think you will have a brief idea of the DMA operation, then we can talk about the detail configuration of the DMA integrate with SPI if you still don't make it.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 06:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418589#M23847</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-05-12T06:21:24Z</dc:date>
    </item>
    <item>
      <title>Re: SPI DMA in SLAVE MODE</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418590#M23848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremyzhou, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got it right. :smileyhappy: I enabled another DMA channel for transmission. Now DMA0 handles SPI reception and DMA1 handles SPI transmission.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Varun R&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2015 09:17:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-DMA-in-SLAVE-MODE/m-p/418590#M23848</guid>
      <dc:creator>varunrajarangan</dc:creator>
      <dc:date>2015-05-12T09:17:22Z</dc:date>
    </item>
  </channel>
</rss>