<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollersのトピックmbed bootloader error for K22 Freedom board</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mbed-bootloader-error-for-K22-Freedom-board/m-p/418046#M23799</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What is the difference between the generic mbed bootloader and the bootloader on the freedom board? I used appendix b of the DOC-100720 to put the bootloader on a K22 freedom board. It went on and started up just fine. Then I MSD'd the 0221_k20dx128_k22f_0x8000.bin file on after which the status light blinked fast which I assume was indicating an error. It did not start after that for an normal power on boot. I've done that on both a freedom board and my own pcb. Any ideas. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jul 2015 16:13:54 GMT</pubDate>
    <dc:creator>jonbuckman</dc:creator>
    <dc:date>2015-07-16T16:13:54Z</dc:date>
    <item>
      <title>mbed bootloader error for K22 Freedom board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mbed-bootloader-error-for-K22-Freedom-board/m-p/418046#M23799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;What is the difference between the generic mbed bootloader and the bootloader on the freedom board? I used appendix b of the DOC-100720 to put the bootloader on a K22 freedom board. It went on and started up just fine. Then I MSD'd the 0221_k20dx128_k22f_0x8000.bin file on after which the status light blinked fast which I assume was indicating an error. It did not start after that for an normal power on boot. I've done that on both a freedom board and my own pcb. Any ideas. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2015 16:13:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mbed-bootloader-error-for-K22-Freedom-board/m-p/418046#M23799</guid>
      <dc:creator>jonbuckman</dc:creator>
      <dc:date>2015-07-16T16:13:54Z</dc:date>
    </item>
  </channel>
</rss>