<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックPTA0/CMP0_IN2 input to comparator on KL03</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PTA0-CMP0-IN2-input-to-comparator-on-KL03/m-p/415175#M23617</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello dear Freescale community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having trouble using PTA0 as CMP0_IN2 to the comparator to the input of the comparator. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I see, my program works fine: if I use PTB5/COMP0_IN1, then everything runs fine, however I want to change from PTB5 to PTA0 since I don't want to mess with the NMI.&amp;nbsp; if it is any useful, I am using the 16QFN package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is how my GPIO configuration looks:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //COMPARATOR PINS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Pin PTA0 as comparator (cmp0_in2 --&amp;nbsp; ALT0)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Pin PTB1 as comparator (cmp0_in3 -- default, ALT0 --- No need to configure, but just to be safe.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetPullCmd(PORTB_BASE_PTR, 1u, false);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetPullCmd(PORTA_BASE_PTR, 0u, false);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTB_BASE_PTR, 1u, kPortPinDisabled);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTA_BASE_PTR, 0u, kPortPinDisabled);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetPullCmd(PORTA_BASE_PTR, 2u, false);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTA_BASE_PTR, 2u,kPortMuxAlt2);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the comparator, I am using the driver. and this is how my configuration looks like:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cmp_comparator_config_t comp_config_struct = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .hystersisMode = kCmpHystersisOfLevel3,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .pinoutEnable = true,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .pinoutUnfilteredEnable = true,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .invertEnable = false,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .highSpeedEnable = true,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .risingIntEnable = false,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .fallingIntEnable = false,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .triggerEnable = false,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //.minusChnMux = kCmpInputChn1,&amp;nbsp; //CMP0_1 is located in PTB5&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .minusChnMux = kCmpInputChn2, //CMP0_2 is located in PTA0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .plusChnMux = kCmpInputChn3,&amp;nbsp;&amp;nbsp; //CMP0_3 is located in PTB1&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I just start the comparator like this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; assert( CMP_DRV_Init(BOARD_CMP_INSTANCE, &amp;amp;comp_state, &amp;amp;comp_config_struct) ==&amp;nbsp; kStatus_CMP_Success);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; CMP_DRV_Start(BOARD_CMP_INSTANCE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debugging is of course a pain since PTA0 uses SWD_CLK, so&amp;nbsp; as soon as I reach that point, I loose debugging capabilities.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice would be really appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jul 2015 15:39:01 GMT</pubDate>
    <dc:creator>carlostadeoorte</dc:creator>
    <dc:date>2015-07-15T15:39:01Z</dc:date>
    <item>
      <title>PTA0/CMP0_IN2 input to comparator on KL03</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PTA0-CMP0-IN2-input-to-comparator-on-KL03/m-p/415175#M23617</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello dear Freescale community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am having trouble using PTA0 as CMP0_IN2 to the comparator to the input of the comparator. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as I see, my program works fine: if I use PTB5/COMP0_IN1, then everything runs fine, however I want to change from PTB5 to PTA0 since I don't want to mess with the NMI.&amp;nbsp; if it is any useful, I am using the 16QFN package.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is how my GPIO configuration looks:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //COMPARATOR PINS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Pin PTA0 as comparator (cmp0_in2 --&amp;nbsp; ALT0)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //Pin PTB1 as comparator (cmp0_in3 -- default, ALT0 --- No need to configure, but just to be safe.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetPullCmd(PORTB_BASE_PTR, 1u, false);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetPullCmd(PORTA_BASE_PTR, 0u, false);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTB_BASE_PTR, 1u, kPortPinDisabled);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTA_BASE_PTR, 0u, kPortPinDisabled);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetPullCmd(PORTA_BASE_PTR, 2u, false);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PORT_HAL_SetMuxMode(PORTA_BASE_PTR, 2u,kPortMuxAlt2);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the comparator, I am using the driver. and this is how my configuration looks like:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cmp_comparator_config_t comp_config_struct = {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .hystersisMode = kCmpHystersisOfLevel3,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .pinoutEnable = true,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .pinoutUnfilteredEnable = true,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .invertEnable = false,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .highSpeedEnable = true,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .risingIntEnable = false,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .fallingIntEnable = false,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .triggerEnable = false,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; //.minusChnMux = kCmpInputChn1,&amp;nbsp; //CMP0_1 is located in PTB5&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .minusChnMux = kCmpInputChn2, //CMP0_2 is located in PTA0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; .plusChnMux = kCmpInputChn3,&amp;nbsp;&amp;nbsp; //CMP0_3 is located in PTB1&lt;/P&gt;&lt;P&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then I just start the comparator like this:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; assert( CMP_DRV_Init(BOARD_CMP_INSTANCE, &amp;amp;comp_state, &amp;amp;comp_config_struct) ==&amp;nbsp; kStatus_CMP_Success);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; CMP_DRV_Start(BOARD_CMP_INSTANCE);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Debugging is of course a pain since PTA0 uses SWD_CLK, so&amp;nbsp; as soon as I reach that point, I loose debugging capabilities.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice would be really appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 15:39:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PTA0-CMP0-IN2-input-to-comparator-on-KL03/m-p/415175#M23617</guid>
      <dc:creator>carlostadeoorte</dc:creator>
      <dc:date>2015-07-15T15:39:01Z</dc:date>
    </item>
    <item>
      <title>Re: PTA0/CMP0_IN2 input to comparator on KL03</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PTA0-CMP0-IN2-input-to-comparator-on-KL03/m-p/415176#M23618</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just as a a follow-up. The code above works perfectly fine, The error was somewhere else in the code where I'd set PTA0 as GPIO&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 19:43:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PTA0-CMP0-IN2-input-to-comparator-on-KL03/m-p/415176#M23618</guid>
      <dc:creator>carlostadeoorte</dc:creator>
      <dc:date>2015-07-15T19:43:06Z</dc:date>
    </item>
    <item>
      <title>Re: PTA0/CMP0_IN2 input to comparator on KL03</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/PTA0-CMP0-IN2-input-to-comparator-on-KL03/m-p/415177#M23619</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Besides of above PTA0 pin MUX setting, it also need to change the &amp;lt;board.h&amp;gt; about BOARD_CMP_CHANNEL&amp;nbsp; definition:&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;#define BOARD_CMP_CHANNEL&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;2 &lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;The KL03 PTA0 pin is CMP0_IN2.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2015 05:45:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/PTA0-CMP0-IN2-input-to-comparator-on-KL03/m-p/415177#M23619</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-07-16T05:45:15Z</dc:date>
    </item>
  </channel>
</rss>