<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPTMR Current in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPTMR-Current/m-p/414653#M23584</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hm, not directely - I would like to know the same information about current usage over temperature range as it is available in Table 10 of the Datadheet "Kinetis KL25 Sub-Family" about the RTC (I_RTC) but for the LPTMR peripheral.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The discription for the RTC is the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"RTC peripheral adder measured by placing the device in VLLS1 mode with external 32 kHz crystal enabled by means of the RTC_CR[OSCE] bit and the RTC ALARM set for 1 minute. Includes ERCLK32K (32 kHz external crystal) power consumption."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with the values: -40C -&amp;gt; 432nA, 25C -&amp;gt; 357na, 50C -&amp;gt; 388na, 70C -&amp;gt; 475na, 85C -&amp;gt; 532na, 105C -&amp;gt; 810na&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the LPTMR the discription could be:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPTMR peripheral adder measured by placing the device in VLLS1 mode with external 32 kHz crystal enabled by means of the RTC_CR[OSCE] bit. Includes ERCLK32K (32 kHz external crystal) power consumption."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with the values: -40C -&amp;gt; XnA, 25C -&amp;gt; Xna, 50C -&amp;gt; Xna, 70C -&amp;gt; Xna, 85C -&amp;gt; Xna, 105C -&amp;gt; Xna&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This information is available for TMP, UART, RTC, CMP ... but not for LPTMR event if the LPTMR can bu used in all Very-Low-Power modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope you understand my issue :-) Thank you and best regards, Dominic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 05 Jun 2015 11:11:01 GMT</pubDate>
    <dc:creator>astdom01</dc:creator>
    <dc:date>2015-06-05T11:11:01Z</dc:date>
    <item>
      <title>LPTMR Current</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPTMR-Current/m-p/414651#M23582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am looking for the power consumption of the LPTMR peripheral in clocked by ERCLK in a low power mode for the KL25x series. I expected the information in the datasheet in table 10 Low power mode peripheral adders - typical value. But there is only I_TMP mentioned not I_LPTMR. I hope I_LPTMR is much lower then I_TMP!? Is this informatin available somewhere?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanx you for any hint.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards, Dominic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Jun 2015 07:28:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPTMR-Current/m-p/414651#M23582</guid>
      <dc:creator>astdom01</dc:creator>
      <dc:date>2015-06-01T07:28:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPTMR Current</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPTMR-Current/m-p/414652#M23583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Dominic!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just to be clear, are you referring to 32 KHz ERCLK32K?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jun 2015 18:16:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPTMR-Current/m-p/414652#M23583</guid>
      <dc:creator>ericfoote1</dc:creator>
      <dc:date>2015-06-04T18:16:47Z</dc:date>
    </item>
    <item>
      <title>Re: LPTMR Current</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPTMR-Current/m-p/414653#M23584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hm, not directely - I would like to know the same information about current usage over temperature range as it is available in Table 10 of the Datadheet "Kinetis KL25 Sub-Family" about the RTC (I_RTC) but for the LPTMR peripheral.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The discription for the RTC is the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"RTC peripheral adder measured by placing the device in VLLS1 mode with external 32 kHz crystal enabled by means of the RTC_CR[OSCE] bit and the RTC ALARM set for 1 minute. Includes ERCLK32K (32 kHz external crystal) power consumption."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with the values: -40C -&amp;gt; 432nA, 25C -&amp;gt; 357na, 50C -&amp;gt; 388na, 70C -&amp;gt; 475na, 85C -&amp;gt; 532na, 105C -&amp;gt; 810na&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the LPTMR the discription could be:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPTMR peripheral adder measured by placing the device in VLLS1 mode with external 32 kHz crystal enabled by means of the RTC_CR[OSCE] bit. Includes ERCLK32K (32 kHz external crystal) power consumption."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with the values: -40C -&amp;gt; XnA, 25C -&amp;gt; Xna, 50C -&amp;gt; Xna, 70C -&amp;gt; Xna, 85C -&amp;gt; Xna, 105C -&amp;gt; Xna&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This information is available for TMP, UART, RTC, CMP ... but not for LPTMR event if the LPTMR can bu used in all Very-Low-Power modes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope you understand my issue :-) Thank you and best regards, Dominic&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Jun 2015 11:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPTMR-Current/m-p/414653#M23584</guid>
      <dc:creator>astdom01</dc:creator>
      <dc:date>2015-06-05T11:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPTMR Current</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPTMR-Current/m-p/414654#M23585</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dominic,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I came across this. It's from the data sheet for KL27, which also has a Cortex M0+ .&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/25930iBD423DAFBFE882FA/image-size/large?v=v2&amp;amp;px=999" title="LPTMR.JPG" alt="LPTMR.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tested a few cases and arrived at room temperature and achieved similar results.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hopefully this helps you some!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-Eric&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jun 2015 22:03:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LPTMR-Current/m-p/414654#M23585</guid>
      <dc:creator>ericfoote1</dc:creator>
      <dc:date>2015-06-09T22:03:51Z</dc:date>
    </item>
  </channel>
</rss>