<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: MQX or EGUI needs</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-or-EGUI-needs/m-p/414567#M23576</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K70 integrates the LCDC module to connect and manage the LCD. You don't need MQX (RTOS) for using &lt;SPAN&gt;eGUI&lt;/SPAN&gt; (graphic library), you can also use bare metal approach with &lt;SPAN&gt;eGUI&lt;/SPAN&gt;. Using MQX will help in the case you need USB, TCP/IP, file system, etc… apart from the graphic user interface. In that case, for example MQX + MFS (file system) allows you to store graphic resources in external USB, SD card, etc…&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 01 Sep 2015 10:13:43 GMT</pubDate>
    <dc:creator>LuisCasado</dc:creator>
    <dc:date>2015-09-01T10:13:43Z</dc:date>
    <item>
      <title>MQX or EGUI needs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-or-EGUI-needs/m-p/414566#M23575</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I Want to know what the need of eGui.&lt;/P&gt;&lt;P&gt;In my project I have to use LCD via EBI interface(using k70). Is this software required for that.&lt;/P&gt;&lt;P&gt;Currently I'm using bareboard project..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ankur&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 09:59:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-or-EGUI-needs/m-p/414566#M23575</guid>
      <dc:creator>ankurchauhan</dc:creator>
      <dc:date>2015-09-01T09:59:20Z</dc:date>
    </item>
    <item>
      <title>Re: MQX or EGUI needs</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-or-EGUI-needs/m-p/414567#M23576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The K70 integrates the LCDC module to connect and manage the LCD. You don't need MQX (RTOS) for using &lt;SPAN&gt;eGUI&lt;/SPAN&gt; (graphic library), you can also use bare metal approach with &lt;SPAN&gt;eGUI&lt;/SPAN&gt;. Using MQX will help in the case you need USB, TCP/IP, file system, etc… apart from the graphic user interface. In that case, for example MQX + MFS (file system) allows you to store graphic resources in external USB, SD card, etc…&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Luis&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 10:13:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-or-EGUI-needs/m-p/414567#M23576</guid>
      <dc:creator>LuisCasado</dc:creator>
      <dc:date>2015-09-01T10:13:43Z</dc:date>
    </item>
  </channel>
</rss>