<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: OpenSDA, UART</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-UART/m-p/413848#M23522</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steffen Wichersheim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yes, you can use UART to flash the KL03 MCU, because this chip have the kinetis ROM bootloader.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For details, please refer to the Chapter 11 Kinetis ROM Bootloader in&amp;nbsp; the KL03 reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jul 2015 01:21:53 GMT</pubDate>
    <dc:creator>kerryzhou</dc:creator>
    <dc:date>2015-07-16T01:21:53Z</dc:date>
    <item>
      <title>OpenSDA, UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-UART/m-p/413847#M23521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;Hello There,&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;I have another question. It is possible to flash the MCU on FRDM KL03Z motherboard via UART ?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;I have five lines to the target MCU measured with my scope . Currently, only the reset line and SWD_CLK SWD_DIO be used..&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 08:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-UART/m-p/413847#M23521</guid>
      <dc:creator>steffenwickersh</dc:creator>
      <dc:date>2015-07-15T08:28:40Z</dc:date>
    </item>
    <item>
      <title>Re: OpenSDA, UART</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-UART/m-p/413848#M23522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steffen Wichersheim,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Yes, you can use UART to flash the KL03 MCU, because this chip have the kinetis ROM bootloader.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For details, please refer to the Chapter 11 Kinetis ROM Bootloader in&amp;nbsp; the KL03 reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2015 01:21:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-UART/m-p/413848#M23522</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-07-16T01:21:53Z</dc:date>
    </item>
  </channel>
</rss>