<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K02 SysTick ISR</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-SysTick-ISR/m-p/412651#M23427</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have code developed using the for the K02FN64VFM10 in which I am using the SysTick to generate an ISR.&amp;nbsp; On a FRDM-K22F board the code executes and I can see that ISR gets services.&amp;nbsp; However, when I down load it onto the K02 target the code executes but the SysTick ISR is not serviced.&amp;nbsp; I'm not sure why this is happening.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Sep 2015 15:23:31 GMT</pubDate>
    <dc:creator>darwinsmith</dc:creator>
    <dc:date>2015-09-25T15:23:31Z</dc:date>
    <item>
      <title>K02 SysTick ISR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-SysTick-ISR/m-p/412651#M23427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have code developed using the for the K02FN64VFM10 in which I am using the SysTick to generate an ISR.&amp;nbsp; On a FRDM-K22F board the code executes and I can see that ISR gets services.&amp;nbsp; However, when I down load it onto the K02 target the code executes but the SysTick ISR is not serviced.&amp;nbsp; I'm not sure why this is happening.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Sep 2015 15:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-SysTick-ISR/m-p/412651#M23427</guid>
      <dc:creator>darwinsmith</dc:creator>
      <dc:date>2015-09-25T15:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: K02 SysTick ISR</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-SysTick-ISR/m-p/412652#M23428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Darwin Smith:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I guess you are using a custom board for the K02. If that is the case please revise that the NMI pin (PTA4) is not in low state by an external signal during Power-ON / Reset. If possible place a pull up resistor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then also related to the NMI pin there could be an issue in debug mode, see this document by colleague Alistair:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-244787"&gt;Interrupts appear to be disabled when debugging.pdf&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let us know if the issue persists.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Jorge Gonzalez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Sep 2015 17:03:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K02-SysTick-ISR/m-p/412652#M23428</guid>
      <dc:creator>Jorge_Gonzalez</dc:creator>
      <dc:date>2015-09-29T17:03:42Z</dc:date>
    </item>
  </channel>
</rss>