<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 High-current failure in KL26</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/High-current-failure-in-KL26/m-p/411590#M23287</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got a couple devices using MKL26Z128VFM4s that have failed in a way that causes the uC to repeatably draw very large (&amp;gt;1A, given enough power supply) currents as soon as power is supplied.&amp;nbsp; I don't know what events might have preceded the initial failure (they were out of my hands at the time), but I had two suspicions: floating inputs and a weak overvoltage on an input pin.&amp;nbsp; The input overvoltage was limited to VCC+0.9V and could only have supplied about 50uA, and applying the same conditions to other devices for extended durations has not replicated the failure.&amp;nbsp; There are also a couple unused pins, and I don't know what could have been going on with those.&amp;nbsp; When the first one happened, I suspected ESD, but then a second one came back to my bench with similar symptoms so I expect it's something more deterministic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody know what sort of conditions might damage a chip like that?&amp;nbsp; I did find that if I supply enough power, in the brief moment before it gets dangerously hot, at least one of the KL26s still executes its code and responds to SWD.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 19 Oct 2015 18:20:26 GMT</pubDate>
    <dc:creator>brianbezanson</dc:creator>
    <dc:date>2015-10-19T18:20:26Z</dc:date>
    <item>
      <title>High-current failure in KL26</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/High-current-failure-in-KL26/m-p/411590#M23287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've got a couple devices using MKL26Z128VFM4s that have failed in a way that causes the uC to repeatably draw very large (&amp;gt;1A, given enough power supply) currents as soon as power is supplied.&amp;nbsp; I don't know what events might have preceded the initial failure (they were out of my hands at the time), but I had two suspicions: floating inputs and a weak overvoltage on an input pin.&amp;nbsp; The input overvoltage was limited to VCC+0.9V and could only have supplied about 50uA, and applying the same conditions to other devices for extended durations has not replicated the failure.&amp;nbsp; There are also a couple unused pins, and I don't know what could have been going on with those.&amp;nbsp; When the first one happened, I suspected ESD, but then a second one came back to my bench with similar symptoms so I expect it's something more deterministic.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anybody know what sort of conditions might damage a chip like that?&amp;nbsp; I did find that if I supply enough power, in the brief moment before it gets dangerously hot, at least one of the KL26s still executes its code and responds to SWD.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Oct 2015 18:20:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/High-current-failure-in-KL26/m-p/411590#M23287</guid>
      <dc:creator>brianbezanson</dc:creator>
      <dc:date>2015-10-19T18:20:26Z</dc:date>
    </item>
    <item>
      <title>Re: High-current failure in KL26</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/High-current-failure-in-KL26/m-p/411591#M23288</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Brain,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the failure of the Kl26, it is difficult to give the concrete cause, I only give you some clue. If you input over-voltage on the input pin of analog or digital pins, you should connect a serial resistor so that the input current is limited less than 2mA. but I do not think the over_voltage on the input pin can leads to the failure of the processor, pls check the power supply pins, each power supply pins should be connect a 0.1uF capacitor.&lt;/P&gt;&lt;P&gt;If possible, you can contact local FAE to do failure analysis to track the cause.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 05:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/High-current-failure-in-KL26/m-p/411591#M23288</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-10-21T05:34:26Z</dc:date>
    </item>
  </channel>
</rss>