<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: KL02 Input voltage operating requirements</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Input-voltage-operating-requirements/m-p/410377#M23143</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Earl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks your feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I know, From theory, the I/O cell is an CMOS circuit, Does the a middle voltage will turn on both MOS gate which will leads to damage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any suggestions to address this issue? &lt;/P&gt;&lt;P&gt;What if we have an logic I/O to the KL02, but the slew rate of the signal is a bit slow, will there be an issue for the VIH/VIL?&lt;/P&gt;&lt;P&gt; If so, what is the acceptable slew rate for the I/O ports in your device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 02 Sep 2015 08:41:39 GMT</pubDate>
    <dc:creator>kriske</dc:creator>
    <dc:date>2015-09-02T08:41:39Z</dc:date>
    <item>
      <title>KL02 Input voltage operating requirements</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Input-voltage-operating-requirements/m-p/410375#M23141</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please help to confirm the below questions,&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;1) The below waveform is our test waveform, and the test condition is:&lt;/LI&gt;&lt;LI&gt;Ch1 is input signal to pin11, and Ch2 is output signal from pin22&lt;/LI&gt;&lt;LI&gt;Pin11 and pin22 are configured GPIO&lt;/LI&gt;&lt;LI&gt;The logic level of Ch2 is the same with Ch1. For example, if Ch1 goes high, then Ch2 goes high too.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52914iAFEA8D24FD5BA7A4/image-size/large?v=v2&amp;amp;px=999" title="未命名.png" alt="未命名.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52950iA2517BE22968E02B/image-size/large?v=v2&amp;amp;px=999" title="DSC_0437.JPG" alt="DSC_0437.JPG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From the datasheet, the input high voltage of KL02 device is about 3.3V * 0.7 = 2.31V.&lt;/P&gt;&lt;P&gt;But, according to our experiment, the output signal goes high even the input signal is about 1.43V ~ 1.89V. Please help to check the input high/low voltage level.&lt;/P&gt;&lt;P&gt;The CH1 max voltage is 1.89V, min voltage is 1.43V, it's available without this voltage range.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52977i92CABC44A82FFA39/image-size/large?v=v2&amp;amp;px=999" title="03.png" alt="03.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please help to confirm input high/low voltage level first, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 10:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Input-voltage-operating-requirements/m-p/410375#M23141</guid>
      <dc:creator>kriske</dc:creator>
      <dc:date>2015-08-31T10:15:26Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Input voltage operating requirements</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Input-voltage-operating-requirements/m-p/410376#M23142</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kris,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recreated the scenario and as you can see in the image shown below, I found very similar results&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/53024i4B815B7291C99B13/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.jpg" alt="pastedImage_0.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The rising edge will toggle the pin's input buffer at about 0.7 * VDD Volts while the falling edge will toggle the input buffer at about 0.35 * VDD Volts. These are the actual input buffer transition points, also known as threshold voltages. The VIL and VIH calculations are to guarantee logic levels – the switch points are well within the VIL/VIH specs. The input buffer thresholds change with VDD, temp, and process, so we cannot guarantee the switchpoint voltages, however, they are within the VIL/VIH limits. And, the difference between the switchpoints will be at least as much as the hysteresis spec, which is about 200mV at VDD = 3.3V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if this information is useful or if I can do anything else for you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl Orlando.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="color: #eb7a3d;"&gt;/* If this post answers your question please click the &lt;SPAN style="text-decoration: underline;"&gt;Correct Answer&lt;/SPAN&gt; button. */&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 22:59:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Input-voltage-operating-requirements/m-p/410376#M23142</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2015-09-01T22:59:26Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Input voltage operating requirements</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Input-voltage-operating-requirements/m-p/410377#M23143</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Earl&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks your feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As I know, From theory, the I/O cell is an CMOS circuit, Does the a middle voltage will turn on both MOS gate which will leads to damage?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any suggestions to address this issue? &lt;/P&gt;&lt;P&gt;What if we have an logic I/O to the KL02, but the slew rate of the signal is a bit slow, will there be an issue for the VIH/VIL?&lt;/P&gt;&lt;P&gt; If so, what is the acceptable slew rate for the I/O ports in your device.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Sep 2015 08:41:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Input-voltage-operating-requirements/m-p/410377#M23143</guid>
      <dc:creator>kriske</dc:creator>
      <dc:date>2015-09-02T08:41:39Z</dc:date>
    </item>
    <item>
      <title>Re: KL02 Input voltage operating requirements</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Input-voltage-operating-requirements/m-p/410378#M23144</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Kris,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am sorry for the delay on my part. The middle voltage range does not damage the I/O cell. The only one issue that you could experiment is the change of the thresholds to toggle from low to high and vice-versa.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Earl.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 16:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL02-Input-voltage-operating-requirements/m-p/410378#M23144</guid>
      <dc:creator>EarlOrlando</dc:creator>
      <dc:date>2015-09-08T16:36:54Z</dc:date>
    </item>
  </channel>
</rss>