<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Slave spi without CS</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Slave-spi-without-CS/m-p/410045#M23089</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As SPI slave, it could not using a GPIO pin instead of SPI slave SS pin function.&lt;/P&gt;&lt;P&gt;While, customer can consider to use four GPIO pins emulate SPI slave communication interface.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Apr 2015 09:25:11 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-04-16T09:25:11Z</dc:date>
    <item>
      <title>Slave spi without CS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Slave-spi-without-CS/m-p/410044#M23088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning&lt;/P&gt;&lt;P&gt;I have a slave SPI working correctly. I would like to emulate the SSI functionality, just getting rid of the CS activation.&lt;/P&gt;&lt;P&gt;It should reset the communication if the clock for some reason stops during the serialization, being ready to begin from the &lt;/P&gt;&lt;P&gt;first bit at next incoming clock pulse.. Is there a suggestion??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank You&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2015 07:40:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Slave-spi-without-CS/m-p/410044#M23088</guid>
      <dc:creator>pietrodicastri</dc:creator>
      <dc:date>2015-04-15T07:40:01Z</dc:date>
    </item>
    <item>
      <title>Re: Slave spi without CS</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Slave-spi-without-CS/m-p/410045#M23089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As SPI slave, it could not using a GPIO pin instead of SPI slave SS pin function.&lt;/P&gt;&lt;P&gt;While, customer can consider to use four GPIO pins emulate SPI slave communication interface.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Apr 2015 09:25:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Slave-spi-without-CS/m-p/410045#M23089</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-04-16T09:25:11Z</dc:date>
    </item>
  </channel>
</rss>