<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMK02 UART in single-wire mode</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-UART-in-single-wire-mode/m-p/409698#M23055</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the MK02 UART in single-wire mode.&amp;nbsp; I think understand that this means setting the UART TX PCR&amp;nbsp; pin registeras a UART Tx pin, and setting the LOOPS and RSRC bits in the UART.&amp;nbsp; Should the pullups be enabled on the Tx pin?&amp;nbsp; Is this bit automatically configured as open drain? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Aug 2015 21:59:21 GMT</pubDate>
    <dc:creator>bruceweyrauch</dc:creator>
    <dc:date>2015-08-31T21:59:21Z</dc:date>
    <item>
      <title>MK02 UART in single-wire mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-UART-in-single-wire-mode/m-p/409698#M23055</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to use the MK02 UART in single-wire mode.&amp;nbsp; I think understand that this means setting the UART TX PCR&amp;nbsp; pin registeras a UART Tx pin, and setting the LOOPS and RSRC bits in the UART.&amp;nbsp; Should the pullups be enabled on the Tx pin?&amp;nbsp; Is this bit automatically configured as open drain? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Aug 2015 21:59:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-UART-in-single-wire-mode/m-p/409698#M23055</guid>
      <dc:creator>bruceweyrauch</dc:creator>
      <dc:date>2015-08-31T21:59:21Z</dc:date>
    </item>
    <item>
      <title>Re: MK02 UART in single-wire mode</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-UART-in-single-wire-mode/m-p/409699#M23056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Bruce&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you are correct. You need to set UART TX PCR to UART function. And enable single wire operation by setting C1[LOOPS] and the receiver source field,&lt;/P&gt;&lt;P&gt;C1[RSRC]. Setting C1[LOOPS] disables the path from the unsynchronized receiver input signal to the receiver. Setting C1[RSRC] connects the receiver input to the output of the TXD pin driver. Both the transmitter and receiver must be enabled (C2[TE] = 1 and C2[RE] = 1).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is no need to set TX pin pull-up and open drain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Sep 2015 06:15:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK02-UART-in-single-wire-mode/m-p/409699#M23056</guid>
      <dc:creator>Paul_Tian</dc:creator>
      <dc:date>2015-09-01T06:15:33Z</dc:date>
    </item>
  </channel>
</rss>