<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: mkm34 PLL or FLL</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkm34-PLL-or-FLL/m-p/408241#M22935</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Edriano,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that you want to get a stable tick for the quadTimer, the quadtimer can get a external clock from crossbar as it's primary clock source. Pls refer to the following part I copy from MKM34RM. In other words, you can connect a clock source from XBAR_IN0~XBAR_IN8 external pins and route the clock source to primary clock via crossbar. From example, you can connect the clock source to pin PTD0/PXBAR_IN2...., while you can set the crossbar as:&lt;/P&gt;&lt;P&gt;XBAR_SEL4|=0x02&amp;lt;&amp;lt;8; it is okay. &lt;/P&gt;&lt;P&gt;I never have test on my board, but I never have a test for the solution, pls have&amp;nbsp; a try.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4581i76F15874FC176D4B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Nov 2015 08:05:53 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2015-11-20T08:05:53Z</dc:date>
    <item>
      <title>mkm34 PLL or FLL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkm34-PLL-or-FLL/m-p/408240#M22934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Currently i am developing an Flowmeter with mkm34 75MHz.&lt;/P&gt;&lt;P&gt;And i am trying to understand what would be the best option as clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In your opinion wich one is more stable PLL or FLL in this microcontroller?&lt;/P&gt;&lt;P&gt;As i could see the PLL needs to have an reference about 32khz is that right? i will not be able to multiply the high frequency xtal oscillator in this case?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Last Does anyone have examples on hou to achieve FEE and PEE using external xtal? i do not intend to use KSDK and i like to understand what is happening &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Nov 2015 13:58:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkm34-PLL-or-FLL/m-p/408240#M22934</guid>
      <dc:creator>Edrianocarlos</dc:creator>
      <dc:date>2015-11-12T13:58:49Z</dc:date>
    </item>
    <item>
      <title>Re: mkm34 PLL or FLL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkm34-PLL-or-FLL/m-p/408241#M22935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Edriano,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see that you want to get a stable tick for the quadTimer, the quadtimer can get a external clock from crossbar as it's primary clock source. Pls refer to the following part I copy from MKM34RM. In other words, you can connect a clock source from XBAR_IN0~XBAR_IN8 external pins and route the clock source to primary clock via crossbar. From example, you can connect the clock source to pin PTD0/PXBAR_IN2...., while you can set the crossbar as:&lt;/P&gt;&lt;P&gt;XBAR_SEL4|=0x02&amp;lt;&amp;lt;8; it is okay. &lt;/P&gt;&lt;P&gt;I never have test on my board, but I never have a test for the solution, pls have&amp;nbsp; a try.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4581i76F15874FC176D4B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 08:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkm34-PLL-or-FLL/m-p/408241#M22935</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-11-20T08:05:53Z</dc:date>
    </item>
    <item>
      <title>Re: mkm34 PLL or FLL</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkm34-PLL-or-FLL/m-p/408242#M22936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I forget to tell you that you have to set the SIM_MISC_CTL to select the IP_BUS, or clock from crossbar as the primary clock for quadTimer..&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Nov 2015 08:21:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/mkm34-PLL-or-FLL/m-p/408242#M22936</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-11-20T08:21:03Z</dc:date>
    </item>
  </channel>
</rss>