<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Kinetis Bootloader 1.2 not working with TWR-MKV31F51212 in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-1-2-not-working-with-TWR-MKV31F51212/m-p/407653#M22858</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Steven&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There is a KBOOT binary for the TWR-KV31F120M (and an application) at &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.utasker.com/kinetis/TWR-KV31F120M.html" rel="nofollow"&gt;http://www.utasker.com/kinetis/TWR-KV31F120M.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Check that it works on your board to ensure that you have no HW problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Nov 2015 23:35:40 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2015-11-12T23:35:40Z</dc:date>
    <item>
      <title>Kinetis Bootloader 1.2 not working with TWR-MKV31F51212</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-1-2-not-working-with-TWR-MKV31F51212/m-p/407652#M22857</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have tested this now with a MK22F51212 Tower and this MKV31.&amp;nbsp; The K22 worked just fine.&amp;nbsp; I basically followed the attached Demo App User's Guide using both boards.&amp;nbsp; The bootloader itself flashes properly to both.&amp;nbsp; I am able to use blhost.exe with both and use the get-property 1 command and get a valid response from both.&amp;nbsp; The issue lies with Figure 10, Section 5.7.&amp;nbsp; I set the image and offset for the two boards (I am sure to use the correct led_demo binary for the proper eval board) and upon pressing update, the K22 erases the flash and writes the led_demo image and works properly while the KV31 can not get past erasing flash and instead I am greeted with "No response packet from target device.".&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Nov 2015 20:51:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-1-2-not-working-with-TWR-MKV31F51212/m-p/407652#M22857</guid>
      <dc:creator>stevenneves</dc:creator>
      <dc:date>2015-11-12T20:51:25Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Bootloader 1.2 not working with TWR-MKV31F51212</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-1-2-not-working-with-TWR-MKV31F51212/m-p/407653#M22858</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Steven&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;There is a KBOOT binary for the TWR-KV31F120M (and an application) at &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://www.utasker.com/kinetis/TWR-KV31F120M.html" rel="nofollow"&gt;http://www.utasker.com/kinetis/TWR-KV31F120M.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Check that it works on your board to ensure that you have no HW problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Nov 2015 23:35:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-1-2-not-working-with-TWR-MKV31F51212/m-p/407653#M22858</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-11-12T23:35:40Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Bootloader 1.2 not working with TWR-MKV31F51212</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-1-2-not-working-with-TWR-MKV31F51212/m-p/407654#M22859</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Steven,&lt;/P&gt;&lt;P&gt;I was wonder if you can share the version of TWR-KV31F120M and specific product number of the KV31.&lt;/P&gt;&lt;P&gt;And I'd also like to know which line of code stucks in when you debug the tower_bootloader demo from the Kinetis_Bootloader_1_2_0.&lt;/P&gt;&lt;P&gt;I'm looking forward to your reply.&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ping&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2015-11-16_17-22-10.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/29821i508B1A68801F7DE7/image-size/large?v=v2&amp;amp;px=999" role="button" title="2015-11-16_17-22-10.jpg" alt="2015-11-16_17-22-10.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Nov 2015 09:21:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Bootloader-1-2-not-working-with-TWR-MKV31F51212/m-p/407654#M22859</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2015-11-16T09:21:45Z</dc:date>
    </item>
  </channel>
</rss>