<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FRDM-K64F losing program after power off in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405442#M22629</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I thought I was using the segger loader, do you have a link to the one you are using? It's from the segger website I assume.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 May 2015 14:18:47 GMT</pubDate>
    <dc:creator>jasondark</dc:creator>
    <dc:date>2015-05-06T14:18:47Z</dc:date>
    <item>
      <title>FRDM-K64F losing program after power off</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405439#M22626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the FRDM-K64F for a senior design project. I am programming the controller using KDS and processor expert by way of OpenSDAv2 from the segger website. I am programming the microcontroller with low level components instead of using the specified freedom board library. When I disconnect the board after debugging, the program only works until it loses power a second time. Any idea why it will not stay programmed indefinitely?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 13:43:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405439#M22626</guid>
      <dc:creator>jasondark</dc:creator>
      <dc:date>2015-05-06T13:43:47Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F losing program after power off</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405440#M22627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm aware of a booting problem with the EZPORT enabled. Maybe this is your issue?&lt;/P&gt;&lt;P&gt;See&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/336449"&gt;FW does not run without SW1 reset after PowerOn&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/332195"&gt;FRDM-K64F booting issue when powered from USB port&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 13:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405440#M22627</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-05-06T13:49:27Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F losing program after power off</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405441#M22628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had this kind of problem when using the default bootloader (from mbed.org).&lt;BR /&gt;Installing the JSegger bootloader solved the problem. And it is also much faster.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Giacomo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 14:07:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405441#M22628</guid>
      <dc:creator>giacomopetrini</dc:creator>
      <dc:date>2015-05-06T14:07:56Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F losing program after power off</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405442#M22629</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I thought I was using the segger loader, do you have a link to the one you are using? It's from the segger website I assume.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 14:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405442#M22629</guid>
      <dc:creator>jasondark</dc:creator>
      <dc:date>2015-05-06T14:18:47Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F losing program after power off</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405443#M22630</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;After reading through the past threads, it is possible to make a software fix for this, correct? My question, is it as simple as changing a value in the flash configuration settings (per a reply to "&lt;STRONG style="font-size: 13px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d;"&gt;&lt;A _jive_internal="true" class="font-color-meta-light" data-content-finding="Community" href="https://community.nxp.com/message/463167#463167" style="font-weight: inherit; font-style: inherit; font-family: inherit; color: #a9a9a9;"&gt;FRDM-K64F booting issue when powered from USB port&lt;/A&gt;&lt;/STRONG&gt;") or do I need to mess with the NMI and have it setup something (also mentioned in the post) Right now, I took all of the button inputs and used them for test inputs, thus disabling the NMI; however, enabling the NMI is not an issue, I guess I just do not fully understand what should be my end goal. Should I just read up more on the EZPORT mode in the reference manual?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 14:25:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405443#M22630</guid>
      <dc:creator>jasondark</dc:creator>
      <dc:date>2015-05-06T14:25:57Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F losing program after power off</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405444#M22631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is an option in the Processor Expert (CPU component) to disable EZPORT:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49361i7DE56E525F3B79FB/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;You could give that one a try.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 14:48:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405444#M22631</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-05-06T14:48:22Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F losing program after power off</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405445#M22632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tried this.. it still would not solve the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2015 15:06:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405445#M22632</guid>
      <dc:creator>jasondark</dc:creator>
      <dc:date>2015-05-07T15:06:54Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F losing program after power off</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405446#M22633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that issue be fixed? What's your FRDM-K64F board hardware version?&lt;/P&gt;&lt;P&gt;Please check the &lt;A href="http://cache.freescale.com/files/32bit/doc/errata/FRDMK64F_ERRATA.pdf"&gt;FRDM-K64f board errata&lt;/A&gt; file.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2015 07:14:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405446#M22633</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-05-14T07:14:32Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-K64F losing program after power off</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405447#M22634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the selected processor expert component can u check if u have selected Flash or RAM for coding. By default the processor expert selects RAM so In that case, it can erase the program on POR. Try selecting Flash .Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Amit&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 May 2015 06:24:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-K64F-losing-program-after-power-off/m-p/405447#M22634</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2015-05-19T06:24:14Z</dc:date>
    </item>
  </channel>
</rss>