<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K65 USB HS without PHY</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-USB-HS-without-PHY/m-p/405242#M22594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think customer can use K65 HS USB without embedded PHY.&lt;/P&gt;&lt;P&gt;It doesn't provides a ULPI interface as normal K70 USB HS module, it have to use the internal PHY for K65 USB HS.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 29 May 2015 06:13:28 GMT</pubDate>
    <dc:creator>Hui_Ma</dc:creator>
    <dc:date>2015-05-29T06:13:28Z</dc:date>
    <item>
      <title>K65 USB HS without PHY</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-USB-HS-without-PHY/m-p/405241#M22593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a way to run the USB HS controller (USB1) on the K65 without running the PHY?&lt;/P&gt;&lt;P&gt;We do not have an external clock.&amp;nbsp; Can we generate a 480MHz clock for the PHY from the 48MHz internal clock?&lt;/P&gt;&lt;P&gt;Can we just disable HS functionality and run the HS controller in full-speed (without having to wait for the PLL to lock)?&lt;/P&gt;&lt;P&gt;Our USB0 pins are not connected.&amp;nbsp; Is there a way to use the USB FS controller with the USB1 pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 May 2015 15:40:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-USB-HS-without-PHY/m-p/405241#M22593</guid>
      <dc:creator>sam_</dc:creator>
      <dc:date>2015-05-28T15:40:49Z</dc:date>
    </item>
    <item>
      <title>Re: K65 USB HS without PHY</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-USB-HS-without-PHY/m-p/405242#M22594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sam,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't think customer can use K65 HS USB without embedded PHY.&lt;/P&gt;&lt;P&gt;It doesn't provides a ULPI interface as normal K70 USB HS module, it have to use the internal PHY for K65 USB HS.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2015 06:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-USB-HS-without-PHY/m-p/405242#M22594</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-05-29T06:13:28Z</dc:date>
    </item>
    <item>
      <title>Re: K65 USB HS without PHY</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-USB-HS-without-PHY/m-p/405243#M22595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for providing this information.&amp;nbsp; &lt;SPAN style="text-decoration: line-through;"&gt;Does the ULPI interface allow for ignoring the PHY and using an internal clock source instead of the PHY?&amp;nbsp; Is there any way to run the USBHS (USB1) controller without UTMI + PHY?&amp;nbsp; Would ULPI allow for that?&lt;/SPAN&gt;&amp;nbsp; After further reading, my impression is that USB always needs a PHY.&amp;nbsp; USB1.0 used a serial connection to the PHY and USB2.0 uses a parallel connection called UTMI.&amp;nbsp; Does ULPI allow for reverting back to the serial connection of USB1.0 at the cost of only being able to run the PHY in full-speed mode?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't understand the hardware well enough, but is there any way (through register settings) to force the USBHS controller to not need a 480MHz clock?&amp;nbsp; If not, is there any way to get it to use an internal clock as an input to the PHY PLL (instead of the external crystal)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 May 2015 11:46:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-USB-HS-without-PHY/m-p/405243#M22595</guid>
      <dc:creator>sam_</dc:creator>
      <dc:date>2015-05-29T11:46:25Z</dc:date>
    </item>
    <item>
      <title>Re: K65 USB HS without PHY</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-USB-HS-without-PHY/m-p/405244#M22596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1&amp;gt; On-chip UTMI transceiver supports high speed (480 Mbps), full speed, and low speed operation in host mode, and high-speed and full-speed operation in device&lt;/P&gt;&lt;P&gt;mode;&lt;/P&gt;&lt;P&gt;2&amp;gt; Please check below link about the different between ULPI vs. UTMI interface.&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.mentor.com/products/ip/usb/usb20otg/phy_interfaces" title="http://www.mentor.com/products/ip/usb/usb20otg/phy_interfaces"&gt;ULPI Interface Standard for High-Speed USB 2.0 IP Systems - Mentor Graphics&lt;/A&gt; &lt;/P&gt;&lt;P&gt;The USB PHY is integrated a 480MHz PLL, there will generate the 480MHz clock with external reference clock.&lt;/P&gt;&lt;P&gt;Thank you for the attention.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 Jul 2015 06:38:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K65-USB-HS-without-PHY/m-p/405244#M22596</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-07-17T06:38:49Z</dc:date>
    </item>
  </channel>
</rss>