<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Kinetis Flexcan : compatibility with previous version?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191507#M2258</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alberto-g ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I never used the Kinetis or ColdFire Flexcan . About the DSC Flexcan, instead, i've used for at least 4-5 years .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the DSC Flexcan, a messages transmitted is "self received" on an rx mailbox if the ID-masks for that mailbox matches a&amp;nbsp; transmitted ID ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 20 Apr 2011 20:58:32 GMT</pubDate>
    <dc:creator>GottiLuca</dc:creator>
    <dc:date>2011-04-20T20:58:32Z</dc:date>
    <item>
      <title>Kinetis Flexcan : compatibility with previous version?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191503#M2254</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Datasheet report&amp;nbsp; "100% backward compatibility with previous Flexcan version".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I think this is not true by a software point of view.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See for example&amp;nbsp; MC56F8323&amp;nbsp;flexcan module.&lt;/P&gt;&lt;P&gt;Message structure buffer are very different (same bits but in different position).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Registers like FCMAXMB (maximum message buffer) are not present in the Kinetis Flexcan module because are included in other 32 bit-register like CANx_MCR (lower 7 byte).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;And so on.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2011 21:16:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191503#M2254</guid>
      <dc:creator>robertob</dc:creator>
      <dc:date>2011-03-16T21:16:07Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Flexcan : compatibility with previous version?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191504#M2255</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Perhahaps the comment related to the flexcan used on the existing Coldfire MCU families rather than the DSCs&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Mar 2011 23:15:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191504#M2255</guid>
      <dc:creator>freegeek</dc:creator>
      <dc:date>2011-03-17T23:15:45Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Flexcan : compatibility with previous version?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191505#M2256</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That's correct. &amp;nbsp;The FlexCAN modules on the Kinetis devices is a newer but backward compatible version of the controller used on previous 32-bit MCUs. &amp;nbsp;The DSC version of FlexCAN is older and not software compatible with the 32-bit MCU CAN modules.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-mnorman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Mar 2011 21:26:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191505#M2256</guid>
      <dc:creator>mnorman</dc:creator>
      <dc:date>2011-03-18T21:26:39Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Flexcan : compatibility with previous version?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191506#M2257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I recall there was an issue with ColdFire CAN, controller is always self receiving its own tx messages.&lt;/P&gt;&lt;P&gt;DSC works ok.&lt;/P&gt;&lt;P&gt;Does anybody know if this was fixed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Apr 2011 19:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191506#M2257</guid>
      <dc:creator>Alberto_g</dc:creator>
      <dc:date>2011-04-20T19:44:11Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Flexcan : compatibility with previous version?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191507#M2258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Alberto-g ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I never used the Kinetis or ColdFire Flexcan . About the DSC Flexcan, instead, i've used for at least 4-5 years .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;On the DSC Flexcan, a messages transmitted is "self received" on an rx mailbox if the ID-masks for that mailbox matches a&amp;nbsp; transmitted ID ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Apr 2011 20:58:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191507#M2258</guid>
      <dc:creator>GottiLuca</dc:creator>
      <dc:date>2011-04-20T20:58:32Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis Flexcan : compatibility with previous version?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191508#M2259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use CANBus on DSC too and it works as it should. My question was about the new Kinetis, since I had this problem with Coldfire M52235.&lt;/P&gt;&lt;P&gt;I had a quick look at the K60 reference manual. It states:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;17&lt;BR /&gt;SRXDIS&lt;BR /&gt;Self Reception Disable&lt;BR /&gt;This bit defines whether FlexCAN is allowed to receive frames transmitted by itself. If this bit is asserted,&lt;BR /&gt;frames transmitted by the module will not be stored in any MB, regardless if the MB is programmed with&lt;BR /&gt;an ID that matches the transmitted frame, and no interrupt flag or interrupt signal will be generated due to&lt;BR /&gt;the frame reception. This bit can only be written in Freeze mode as it is locked by hardware in other&lt;BR /&gt;modes.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So it seems the issue was addressed. I am waiting for a TWR kit, let's see.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Apr 2011 22:10:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-Flexcan-compatibility-with-previous-version/m-p/191508#M2259</guid>
      <dc:creator>Alberto_g</dc:creator>
      <dc:date>2011-04-20T22:10:30Z</dc:date>
    </item>
  </channel>
</rss>