<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 MKL25Z128 Internal USB 3.3V regulator limitations</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL25Z128-Internal-USB-3-3V-regulator-limitations/m-p/405049#M22554</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use the MKL25Z1128 USB 3.3V regulator to power the MCU, if I don't surpass Iout = 120mA?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marco Coelho&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Sep 2015 21:02:47 GMT</pubDate>
    <dc:creator>MAPC</dc:creator>
    <dc:date>2015-09-23T21:02:47Z</dc:date>
    <item>
      <title>MKL25Z128 Internal USB 3.3V regulator limitations</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL25Z128-Internal-USB-3-3V-regulator-limitations/m-p/405049#M22554</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use the MKL25Z1128 USB 3.3V regulator to power the MCU, if I don't surpass Iout = 120mA?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Marco Coelho&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 21:02:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL25Z128-Internal-USB-3-3V-regulator-limitations/m-p/405049#M22554</guid>
      <dc:creator>MAPC</dc:creator>
      <dc:date>2015-09-23T21:02:47Z</dc:date>
    </item>
    <item>
      <title>Re: MKL25Z128 Internal USB 3.3V regulator limitations</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL25Z128-Internal-USB-3-3V-regulator-limitations/m-p/405050#M22555</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marco,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you can use KL25 USB regulator 3.3V output to power the KL25 chip, please refer the application below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2015-09-24_10-41-35.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57442iCAC4675808E20DD0/image-size/large?v=v2&amp;amp;px=999" role="button" title="2015-09-24_10-41-35.png" alt="2015-09-24_10-41-35.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Sep 2015 02:42:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKL25Z128-Internal-USB-3-3V-regulator-limitations/m-p/405050#M22555</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-09-24T02:42:13Z</dc:date>
    </item>
  </channel>
</rss>