<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K60 series DDR controller</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-series-DDR-controller/m-p/191493#M2253</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nitesh, these are the K60 parts supporting a DDR interface:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MK61FX512VMJ12&lt;/LI&gt;&lt;LI&gt;MK61FN1M0VMJ12&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mini USB connector attached to the WTR-K60xxx boards can only be used to program/debug, however if you are using the complete kit you can attach your USB drive to the TWR-SER USB port.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Oct 2012 17:28:47 GMT</pubDate>
    <dc:creator>apanecatl</dc:creator>
    <dc:date>2012-10-22T17:28:47Z</dc:date>
    <item>
      <title>K60 series DDR controller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-series-DDR-controller/m-p/191492#M2252</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;I am looking for a microcontroller in k60 series which supports ddr controller. I have looked in their K60 product brief where it says that they support DDR controllers but while choosing in the MCU solution advisor , k60 series doesnt feature ?? so I was wondering if anybody can tell me which microcontroller of K60 series supports DDR controller or it doesnt at all&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also does the tower system for K60 support&amp;nbsp; a USB host so as to put in a pen drive etc. , I am trying to figure this out yet.&lt;/P&gt;&lt;P&gt;Please reply&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Aug 2012 15:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-series-DDR-controller/m-p/191492#M2252</guid>
      <dc:creator>mneta</dc:creator>
      <dc:date>2012-08-24T15:15:39Z</dc:date>
    </item>
    <item>
      <title>Re: K60 series DDR controller</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-series-DDR-controller/m-p/191493#M2253</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nitesh, these are the K60 parts supporting a DDR interface:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;MK61FX512VMJ12&lt;/LI&gt;&lt;LI&gt;MK61FN1M0VMJ12&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The mini USB connector attached to the WTR-K60xxx boards can only be used to program/debug, however if you are using the complete kit you can attach your USB drive to the TWR-SER USB port.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Oct 2012 17:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-series-DDR-controller/m-p/191493#M2253</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2012-10-22T17:28:47Z</dc:date>
    </item>
  </channel>
</rss>