<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMK64FN1M0VMD12 tri-state</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FN1M0VMD12-tri-state/m-p/404597#M22519</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I hold the Kinetis MK64FN1M0VMD12 in reset, will the processor go in tri-state mode/high impedance? I couldn't find this in the datasheet (I might have missed it)&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jun 2015 12:30:16 GMT</pubDate>
    <dc:creator>larsarntz</dc:creator>
    <dc:date>2015-06-16T12:30:16Z</dc:date>
    <item>
      <title>MK64FN1M0VMD12 tri-state</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FN1M0VMD12-tri-state/m-p/404597#M22519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I hold the Kinetis MK64FN1M0VMD12 in reset, will the processor go in tri-state mode/high impedance? I couldn't find this in the datasheet (I might have missed it)&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 12:30:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FN1M0VMD12-tri-state/m-p/404597#M22519</guid>
      <dc:creator>larsarntz</dc:creator>
      <dc:date>2015-06-16T12:30:16Z</dc:date>
    </item>
    <item>
      <title>Re: MK64FN1M0VMD12 tri-state</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FN1M0VMD12-tri-state/m-p/404598#M22520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;From K64P144M120SF5RM.pdf:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;55.2.6, the definition for Port Data Direction Registers (GPIOx_PDDR) shows all reset to 'all zero', so that defines all GPIO-mode-pins as 'input' (high impedance).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The next question is 'which pins are GPIO at reset', and for that we jump over to table 10-2, and more particularly 10.3.1 'default' column, to see that 'most port pins' default to&amp;nbsp; the analog-input modes, crystal, or disabled (ALT0).&amp;nbsp; So, NOT GPIO, but high-impedance nonetheless.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jun 2015 15:56:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FN1M0VMD12-tri-state/m-p/404598#M22520</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2015-06-16T15:56:38Z</dc:date>
    </item>
    <item>
      <title>Re: MK64FN1M0VMD12 tri-state</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FN1M0VMD12-tri-state/m-p/404599#M22521</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you expecting more information?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jun 2015 20:35:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FN1M0VMD12-tri-state/m-p/404599#M22521</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2015-06-17T20:35:22Z</dc:date>
    </item>
    <item>
      <title>Re: MK64FN1M0VMD12 tri-state</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FN1M0VMD12-tri-state/m-p/404600#M22522</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;&lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;During&lt;/SPAN&gt; the reset, besides of JTAG pins, EzPort pins, power pins and external oscillator pins are enabled, other pins are high-impedance(disable).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this information can help you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Adrian Sanchez Cano&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jun 2015 01:03:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MK64FN1M0VMD12-tri-state/m-p/404600#M22522</guid>
      <dc:creator>adriancano</dc:creator>
      <dc:date>2015-06-18T01:03:15Z</dc:date>
    </item>
  </channel>
</rss>