<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: kv11 flexcan network example</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kv11-flexcan-network-example/m-p/404136#M22504</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Jason,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, i have not the example code for FlexCan based on Kinetis, but the MC56F84xxx and Kinetis use the same FlexCAN module, I attach the example based on MC56F84xxx, so that you can refer to it.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Nov 2015 03:51:50 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2015-11-17T03:51:50Z</dc:date>
    <item>
      <title>kv11 flexcan network example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kv11-flexcan-network-example/m-p/404135#M22503</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello I am using the KV11 device and KSDK 1.3.&amp;nbsp; I noticed there is no flexcan network example.&amp;nbsp; There was a version started in standalone 1.2 but it did not compile.&amp;nbsp; Is Freescale working on something that they are able to share for demonstrating the flexcan interface on the KV11 device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Jason Haedt&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Nov 2015 02:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kv11-flexcan-network-example/m-p/404135#M22503</guid>
      <dc:creator>jasonhaedt</dc:creator>
      <dc:date>2015-11-12T02:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: kv11 flexcan network example</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/kv11-flexcan-network-example/m-p/404136#M22504</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,Jason,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, i have not the example code for FlexCan based on Kinetis, but the MC56F84xxx and Kinetis use the same FlexCAN module, I attach the example based on MC56F84xxx, so that you can refer to it.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Nov 2015 03:51:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/kv11-flexcan-network-example/m-p/404136#M22504</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2015-11-17T03:51:50Z</dc:date>
    </item>
  </channel>
</rss>