<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 K64F Must use external 50MHz Ethernet clock?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-Must-use-external-50MHz-Ethernet-clock/m-p/402827#M22413</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the K64F MCU capable of generating the 50MHz clock for RMII Ethernet?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to avoid adding a crystal to generate this clock in the PHY.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Jul 2015 23:58:55 GMT</pubDate>
    <dc:creator>joelk</dc:creator>
    <dc:date>2015-07-31T23:58:55Z</dc:date>
    <item>
      <title>K64F Must use external 50MHz Ethernet clock?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-Must-use-external-50MHz-Ethernet-clock/m-p/402827#M22413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is the K64F MCU capable of generating the 50MHz clock for RMII Ethernet?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to avoid adding a crystal to generate this clock in the PHY.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2015 23:58:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-Must-use-external-50MHz-Ethernet-clock/m-p/402827#M22413</guid>
      <dc:creator>joelk</dc:creator>
      <dc:date>2015-07-31T23:58:55Z</dc:date>
    </item>
    <item>
      <title>Re: K64F Must use external 50MHz Ethernet clock?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-Must-use-external-50MHz-Ethernet-clock/m-p/402828#M22414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Joel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You "need" to have a 50MHz clock signal on CLKIN, which is internally connected to the MII clock line, in order to use Ethernet in RMII mode.&lt;/P&gt;&lt;P&gt;There is however no need to have two crystals/clocks due to this - just choose a PHY that accepts a 25MHz crystal and supplies the 50MHz clock to the K64 input (eg. KSZ8081RNA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You just need to allow the PHY to come out of reset so that it can start up and supply the Kinetis clock,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have worked on several K60, K64, K61, K70 products using this strategy and there are no problems - and the only crystal required is the one at the PHY.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;If you have to avoid generating the clock at the PHY you can also use an external 50MHz oscillator - with a PHY requiring the clock as input (as is done on the K60 tower kit). It is important that the same oscillator source is used for both (synchronised).&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kinetis: &lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt; &lt;/P&gt;&lt;P&gt;K64: &lt;A href="http://www.utasker.com/kinetis/FRDM-K64F.html" title="http://www.utasker.com/kinetis/FRDM-K64F.html"&gt;µTasker Kinetis FRDM-K64F support&lt;/A&gt;&amp;nbsp; / &lt;A href="http://www.utasker.com/kinetis/TWR-K64F120M.html" title="http://www.utasker.com/kinetis/TWR-K64F120M.html"&gt;µTasker Kinetis TWR-K64F120M support&lt;/A&gt;&amp;nbsp; / &lt;A href="http://www.utasker.com/kinetis/TWR-K65F180M.html" title="http://www.utasker.com/kinetis/TWR-K65F180M.html"&gt;µTasker Kinetis TWR-K65F180M support&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;EM&gt;For the complete "out-of-the-box" Kinetis experience and faster time to market&lt;/EM&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Aug 2015 16:19:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K64F-Must-use-external-50MHz-Ethernet-clock/m-p/402828#M22414</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-08-01T16:19:57Z</dc:date>
    </item>
  </channel>
</rss>