<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Seeing multiple DTE Activated events - is this normal? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Seeing-multiple-DTE-Activated-events-is-this-normal/m-p/402096#M22366</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Isaac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ended up figuring out the issue and yes it was on the Host terminal side. When I would vary the timeout on the connection on the host, internally, it was doing something that would trigger these events. Many times I would just assert the same port timeout value, but internally it would still generate the event. So, I created a wrapper that would ignore setting the same timeout value and this fixed it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Raj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Oct 2015 23:20:44 GMT</pubDate>
    <dc:creator>rajbatra</dc:creator>
    <dc:date>2015-10-27T23:20:44Z</dc:date>
    <item>
      <title>Seeing multiple DTE Activated events - is this normal?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Seeing-multiple-DTE-Activated-events-is-this-normal/m-p/402094#M22364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using a k64F uP and implemented the USB CDC driver (KSDK+MQX). Up till now, I had been sending 64 bytes of data over the virtual com port and everything has been working fine. When I started sending data that is 280 bytes long, I noticed that I get multiple USB_APP_CDC_DTE_ACTIVATED events. Nothing bad seems to be happening, but am wondering if this is normal? I'm not a USB expert, and not sure if my Windows box is doing a flow control or pacing data - or if something weird is going on that I should be concerned about.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Raj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Oct 2015 00:30:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Seeing-multiple-DTE-Activated-events-is-this-normal/m-p/402094#M22364</guid>
      <dc:creator>rajbatra</dc:creator>
      <dc:date>2015-10-16T00:30:15Z</dc:date>
    </item>
    <item>
      <title>Re: Seeing multiple DTE Activated events - is this normal?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Seeing-multiple-DTE-Activated-events-is-this-normal/m-p/402095#M22365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Raj,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As far as i know, this event is sent from Host terminal. I receive an USB_APP_CDC_DTE_ACTIVATED event every time i open a new terminal when using TeraTerm, but i do not receive more than one event eventhough i received more than 280 bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You should pay attention on your Host terminal rather than USB CDC example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this can help you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Isaac&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Oct 2015 22:48:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Seeing-multiple-DTE-Activated-events-is-this-normal/m-p/402095#M22365</guid>
      <dc:creator>isaacavila</dc:creator>
      <dc:date>2015-10-27T22:48:21Z</dc:date>
    </item>
    <item>
      <title>Re: Seeing multiple DTE Activated events - is this normal?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Seeing-multiple-DTE-Activated-events-is-this-normal/m-p/402096#M22366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Isaac,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ended up figuring out the issue and yes it was on the Host terminal side. When I would vary the timeout on the connection on the host, internally, it was doing something that would trigger these events. Many times I would just assert the same port timeout value, but internally it would still generate the event. So, I created a wrapper that would ignore setting the same timeout value and this fixed it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Raj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Oct 2015 23:20:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Seeing-multiple-DTE-Activated-events-is-this-normal/m-p/402096#M22366</guid>
      <dc:creator>rajbatra</dc:creator>
      <dc:date>2015-10-27T23:20:44Z</dc:date>
    </item>
  </channel>
</rss>