<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCR20A problem with custom board in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCR20A-problem-with-custom-board/m-p/401973#M22349</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used MCR20A Zigbee chip with Zigbee &lt;STRONG&gt;SMAC&lt;/STRONG&gt; stack in my project with &lt;STRONG&gt;MKL26Z256VLH4 &lt;/STRONG&gt;micro controller.&lt;/P&gt;&lt;P&gt;I have used FRDM KL26Z and FRDM - MCR20a development board for my prior testing and development.&lt;/P&gt;&lt;P&gt;Now, I am changed my code according to my custom board.&lt;/P&gt;&lt;P&gt;changes are as below:&lt;/P&gt;&lt;P&gt;1.)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Pin outs changed as per used in custom board.&lt;/P&gt;&lt;P&gt;2.)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI 0 is used in custom board so changed instance and also pins from SPI1 to SPI0.(development board uses SPI1).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Custom board also contains Power amplifier so enabled&lt;STRONG&gt; PA and LNA&lt;/STRONG&gt; control by changing&lt;STRONG&gt; ANT PAD&lt;/STRONG&gt; related register in zigbee SMAC stack( &lt;STRONG&gt;no other changes in stack&lt;/STRONG&gt;).&lt;/P&gt;&lt;P&gt;my code on development board working proper.(transmit and receive both)&lt;/P&gt;&lt;P&gt;But same code with necessary changes not working properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problems are listed below:&lt;/P&gt;&lt;P&gt;1.) Transmit is working but some packets are lost (1 of 10 is lost).&lt;/P&gt;&lt;P&gt;2.) Receive is not working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is my findings and analysis:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) SPI clock of development board is 8 MHZ where as of my custom board is 6 MHZ.&lt;/P&gt;&lt;P&gt;2.) my custom board is working at 2.5 volt.&lt;/P&gt;&lt;P&gt;3.) Whenever i request the data packet to send is gives me an interrupt on IRQ pin but sometimes It does not give an interrupt and that packet is lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so any one could have idea what should be the cause for this problem?&lt;/P&gt;&lt;P&gt;SPI clock rate ?&lt;/P&gt;&lt;P&gt;Voltage?&lt;/P&gt;&lt;P&gt;or any other?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ronak Panchal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Oct 2015 17:34:21 GMT</pubDate>
    <dc:creator>ronakpanchal</dc:creator>
    <dc:date>2015-10-15T17:34:21Z</dc:date>
    <item>
      <title>MCR20A problem with custom board</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCR20A-problem-with-custom-board/m-p/401973#M22349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have used MCR20A Zigbee chip with Zigbee &lt;STRONG&gt;SMAC&lt;/STRONG&gt; stack in my project with &lt;STRONG&gt;MKL26Z256VLH4 &lt;/STRONG&gt;micro controller.&lt;/P&gt;&lt;P&gt;I have used FRDM KL26Z and FRDM - MCR20a development board for my prior testing and development.&lt;/P&gt;&lt;P&gt;Now, I am changed my code according to my custom board.&lt;/P&gt;&lt;P&gt;changes are as below:&lt;/P&gt;&lt;P&gt;1.)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Pin outs changed as per used in custom board.&lt;/P&gt;&lt;P&gt;2.)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SPI 0 is used in custom board so changed instance and also pins from SPI1 to SPI0.(development board uses SPI1).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Custom board also contains Power amplifier so enabled&lt;STRONG&gt; PA and LNA&lt;/STRONG&gt; control by changing&lt;STRONG&gt; ANT PAD&lt;/STRONG&gt; related register in zigbee SMAC stack( &lt;STRONG&gt;no other changes in stack&lt;/STRONG&gt;).&lt;/P&gt;&lt;P&gt;my code on development board working proper.(transmit and receive both)&lt;/P&gt;&lt;P&gt;But same code with necessary changes not working properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problems are listed below:&lt;/P&gt;&lt;P&gt;1.) Transmit is working but some packets are lost (1 of 10 is lost).&lt;/P&gt;&lt;P&gt;2.) Receive is not working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is my findings and analysis:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.) SPI clock of development board is 8 MHZ where as of my custom board is 6 MHZ.&lt;/P&gt;&lt;P&gt;2.) my custom board is working at 2.5 volt.&lt;/P&gt;&lt;P&gt;3.) Whenever i request the data packet to send is gives me an interrupt on IRQ pin but sometimes It does not give an interrupt and that packet is lost.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;so any one could have idea what should be the cause for this problem?&lt;/P&gt;&lt;P&gt;SPI clock rate ?&lt;/P&gt;&lt;P&gt;Voltage?&lt;/P&gt;&lt;P&gt;or any other?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ronak Panchal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2015 17:34:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MCR20A-problem-with-custom-board/m-p/401973#M22349</guid>
      <dc:creator>ronakpanchal</dc:creator>
      <dc:date>2015-10-15T17:34:21Z</dc:date>
    </item>
  </channel>
</rss>