<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Wiriting other half of flash from code in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191374#M2233</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Apparently, yes. Thanks. Disregard thread unless someone else runs into this problem.&lt;/P&gt;&lt;P&gt;Aggravating though that something which used to work on older silicon is now busted.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 20 Dec 2011 08:20:22 GMT</pubDate>
    <dc:creator>comsosysarch</dc:creator>
    <dc:date>2011-12-20T08:20:22Z</dc:date>
    <item>
      <title>Wiriting other half of flash from code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191371#M2230</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;K60 chips with part number PK60N512VLQ100&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I had some code running on three different chips batch marked 0M33Z. Has worked for several motnshs with no changes.&lt;/P&gt;&lt;P&gt;Now we have some chips batch marked 2N30Q.&lt;/P&gt;&lt;P&gt;Same code no longer works on any of the three new devices with that batch marking.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Code with the issue happens to be related to writing to upper half of flash while running from lower half of flash.&lt;/P&gt;&lt;P&gt;These are all flash-only devices (ie no flex).&lt;/P&gt;&lt;P&gt;I am disabling flash caching due to the issue with that on the 0M33Z devices. Then I erase the sector containing the flash table, then writing the new table data to the accelerator block in RAM, then commanding the flash controller to write to flash. This gets repeated as often as needed to fill a table.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It -seems- to (perhaps) work one time, but never after that. The IAR debugger leaves much to be desired for this sort of thing but that would be a whole other story.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any ideas based on what changed in the device between those chip batches?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 06:06:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191371#M2230</guid>
      <dc:creator>comsosysarch</dc:creator>
      <dc:date>2011-12-20T06:06:12Z</dc:date>
    </item>
    <item>
      <title>Re: Wiriting other half of flash from code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191372#M2231</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It looks like I am getting a read collision error on the new chips.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;FTFL Read Collision Error Flag&lt;BR /&gt;The RDCOLERR error bit indicates that the MCU attempted a read from an FTFL resource that was being&lt;BR /&gt;manipulated by an FTFL command (CCIF=0). Any simultaneous access is detected as a collision error by&lt;BR /&gt;the block arbitration logic. The read data in this case cannot be guaranteed. The RDCOLERR bit is&lt;BR /&gt;cleared by writing a 1 to it. Writing a 0 to RDCOLERR has no effect.&lt;BR /&gt;0 No collision error detected&lt;BR /&gt;1 Collision error detected&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Not sure how. Here is the code that is executing when the error occurs. It is directly out of the FRM flowchart.&lt;/P&gt;&lt;PRE&gt;bool ftflErsScr(UInt32 flAddr){ if(flAddr &amp;amp; 0xff000007)  return false; if(flAddr &amp;lt; 0x00040000 || flAddr &amp;gt; 0x0007ffff)  return false; while(!(FTFL_BASE_PTR-&amp;gt;FSTAT &amp;amp; FTFL_FSTAT_CCIF_MASK)); // wait for any previous command to complete (required to proceed) if(FTFL_BASE_PTR-&amp;gt;FSTAT &amp;amp; (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK)) // check for previous command error flags  FTFL_BASE_PTR-&amp;gt;FSTAT = (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK); // write 1 to clear error flags (required to proceed) FTFL_BASE_PTR-&amp;gt;FCCOB0 = 0x09; // erase sector command FTFL_BASE_PTR-&amp;gt;FCCOB1 = (UInt08)((flAddr &amp;amp; 0x00ff0000) &amp;gt;&amp;gt; 16); FTFL_BASE_PTR-&amp;gt;FCCOB2 = (UInt08)((flAddr &amp;amp; 0x0000ff00) &amp;gt;&amp;gt; 8); FTFL_BASE_PTR-&amp;gt;FCCOB3 = (UInt08)(flAddr &amp;amp; 0x000000f8); FTFL_BASE_PTR-&amp;gt;FSTAT = FTFL_FSTAT_CCIF_MASK; // write 1 to clear flag (executes command) while(!(FTFL_BASE_PTR-&amp;gt;FSTAT &amp;amp; FTFL_FSTAT_CCIF_MASK)); // wait for command to complete return((FTFL_BASE_PTR-&amp;gt;FSTAT &amp;amp; (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK | FTFL_FSTAT_MGSTAT0_MASK)) == 0); // return command error flag status}bool ftflPgmSec(UInt32 flAddr, UInt16 num64s){ if(flAddr &amp;amp; 0xff000007)  return false; if(num64s == 0)  return false; if(flAddr &amp;lt; 0x00040000 || flAddr &amp;gt; 0x0007ffff)  return false; while(!(FTFL_BASE_PTR-&amp;gt;FSTAT &amp;amp; FTFL_FSTAT_CCIF_MASK)); // wait for any previous command to complete (required to proceed) if(FTFL_BASE_PTR-&amp;gt;FSTAT &amp;amp; (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK)) // check for previous command error flags  FTFL_BASE_PTR-&amp;gt;FSTAT = (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK); // write 1 to clear error flags (required to proceed) FTFL_BASE_PTR-&amp;gt;FCCOB0 = 0x0b; // program section command FTFL_BASE_PTR-&amp;gt;FCCOB1 = (UInt08)((flAddr &amp;amp; 0x00ff0000) &amp;gt;&amp;gt; 16); FTFL_BASE_PTR-&amp;gt;FCCOB2 = (UInt08)((flAddr &amp;amp; 0x0000ff00) &amp;gt;&amp;gt; 8); FTFL_BASE_PTR-&amp;gt;FCCOB3 = (UInt08)(flAddr &amp;amp; 0x000000f8); FTFL_BASE_PTR-&amp;gt;FCCOB4 = (UInt08)(num64s &amp;gt;&amp;gt; 8); FTFL_BASE_PTR-&amp;gt;FCCOB5 = (UInt08)(num64s &amp;amp; 0x00ff); FTFL_BASE_PTR-&amp;gt;FSTAT = FTFL_FSTAT_CCIF_MASK; // write 1 to clear flag (executes command) while(!(FTFL_BASE_PTR-&amp;gt;FSTAT &amp;amp; FTFL_FSTAT_CCIF_MASK)); // wait for command to complete return((FTFL_BASE_PTR-&amp;gt;FSTAT &amp;amp; (FTFL_FSTAT_ACCERR_MASK | FTFL_FSTAT_FPVIOL_MASK | FTFL_FSTAT_MGSTAT0_MASK)) == 0); // return command error flag status}&lt;/PRE&gt;&lt;P&gt;The erase sector command works fine every time. But the program section generates the read collision while in the last loop waiting for the CCIF bit to be set indicating the completion of the operation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The routine is around flash address 0x15ac2 (lower half). The flash table being programmed is at 0x40000 or 0x50000 (upper half).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:43:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191372#M2231</guid>
      <dc:creator>comsosysarch</dc:creator>
      <dc:date>2020-10-29T09:43:12Z</dc:date>
    </item>
    <item>
      <title>Re: Wiriting other half of flash from code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191373#M2232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The following is in the 2N30D errata. Maybe a new problem in something that used to work on 0M33Z?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;e2596: EzPort and FTFL: The 64-bit flash programming command PGMSEC is not fully&lt;BR /&gt;implemented.&lt;BR /&gt;Errata type: Errata&lt;BR /&gt;Description: The 64-bit flash programming command PGMSEC is not fully implemented. The command can&lt;BR /&gt;be used by flash programming algorithms and is used by the EzPort serial flash programming&lt;BR /&gt;interface.&lt;BR /&gt;Workaround: Use the 32-bit flash programming command PGM4 in flash programming algorithms until the&lt;BR /&gt;PGMSEC command is fully supported. Do not use the EzPort module until PGMSEC is fully&lt;BR /&gt;supported.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If so, do I just need to use PGM4 instead?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 07:30:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191373#M2232</guid>
      <dc:creator>comsosysarch</dc:creator>
      <dc:date>2011-12-20T07:30:45Z</dc:date>
    </item>
    <item>
      <title>Re: Wiriting other half of flash from code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191374#M2233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Apparently, yes. Thanks. Disregard thread unless someone else runs into this problem.&lt;/P&gt;&lt;P&gt;Aggravating though that something which used to work on older silicon is now busted.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Dec 2011 08:20:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191374#M2233</guid>
      <dc:creator>comsosysarch</dc:creator>
      <dc:date>2011-12-20T08:20:22Z</dc:date>
    </item>
    <item>
      <title>Re: Wiriting other half of flash from code</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191375#M2234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Refer also&amp;nbsp;to my thread:&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.freescale.com/message/94076#94076" title="https://community.freescale.com/message/94076#94076"&gt;https://community.freescale.com/message/94076#94076&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Flash bank/swap operations were significantly changed over the silicon revs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;--ERGII&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 31 Dec 2011 08:20:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Wiriting-other-half-of-flash-from-code/m-p/191375#M2234</guid>
      <dc:creator>egoodii</dc:creator>
      <dc:date>2011-12-31T08:20:32Z</dc:date>
    </item>
  </channel>
</rss>