<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックK22_120 VLPS power consumption</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-VLPS-power-consumption/m-p/400061#M22169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am looking at two different members of the K22_120 family, MK22FN512VDC12 and MK22FN1M0VMC12.&amp;nbsp; As far as I can tell from the datasheets these parts are pretty much identical, except that the latter has 1M of FLASH rather than 512k.&amp;nbsp; Yet if I look at the VLPS power consumption for the two parts, the first has a typical figure of 8.7uA, but the second has a typical figure of 78uA, almost 10x greater.&amp;nbsp; I would expect the 1M part to have a slightly higher consumption because of the extra FLASH, but not that much higher.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone explain the reason for the large difference between the two VLPS currents?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Apr 2015 05:06:42 GMT</pubDate>
    <dc:creator>peterrush</dc:creator>
    <dc:date>2015-04-13T05:06:42Z</dc:date>
    <item>
      <title>K22_120 VLPS power consumption</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-VLPS-power-consumption/m-p/400061#M22169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am looking at two different members of the K22_120 family, MK22FN512VDC12 and MK22FN1M0VMC12.&amp;nbsp; As far as I can tell from the datasheets these parts are pretty much identical, except that the latter has 1M of FLASH rather than 512k.&amp;nbsp; Yet if I look at the VLPS power consumption for the two parts, the first has a typical figure of 8.7uA, but the second has a typical figure of 78uA, almost 10x greater.&amp;nbsp; I would expect the 1M part to have a slightly higher consumption because of the extra FLASH, but not that much higher.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone explain the reason for the large difference between the two VLPS currents?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Apr 2015 05:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-VLPS-power-consumption/m-p/400061#M22169</guid>
      <dc:creator>peterrush</dc:creator>
      <dc:date>2015-04-13T05:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: K22_120 VLPS power consumption</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-VLPS-power-consumption/m-p/400062#M22170</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Peter Rush,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Actually, There has a lot of differences between MK22FN512VDC12 and MK22FN1M0VMC12. Besides of the flash size difference, MK22FN1M0VMC12 has more modules than MK22FN512VDC12.&lt;/P&gt;&lt;P&gt;For details, you can refer to this post:&lt;/P&gt;&lt;H1&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-102548"&gt;Kinetis K22_120 MHz devices&lt;/A&gt;&lt;/H1&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;, and the according reference manual.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; In VLPS mode, MK22FN1M0VMC12 is really have higher power consumption thanMK22FN512VDC12, this is just the design, you should refer to our datasheet value.&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2015 05:31:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K22-120-VLPS-power-consumption/m-p/400062#M22170</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-04-14T05:31:52Z</dc:date>
    </item>
  </channel>
</rss>