<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: How to write internal FLASH?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-write-internal-FLASH/m-p/190634#M2213</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is possible to update SW in various manners and this is possibel with the Kinetis devices as with others, such as the M522XX Coldfire ones, which have similar FLASH.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The fact that there are 2 partitions in the larger chips means that it is possible to run code in one plane while executing Flash commands in the other, but this is not a main issue when uploading new code and it is also possible when using device with one Flash plane.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See also: &lt;A href="http://www.utasker.com/docs/uTasker/BM-Booloader_for_M5223X.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/BM-Booloader_for_M5223X.PDF&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 13 Mar 2011 06:43:13 GMT</pubDate>
    <dc:creator>mjbcswitzerland</dc:creator>
    <dc:date>2011-03-13T06:43:13Z</dc:date>
    <item>
      <title>How to write internal FLASH?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-write-internal-FLASH/m-p/190633#M2212</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If my program is running from internal flash memory, and I want to upgrade to a newer version. Is it possible do the upgrade through my program in the filed? I noticed that Kinetis has two partiotion of the Flash.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Mar 2011 23:01:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-write-internal-FLASH/m-p/190633#M2212</guid>
      <dc:creator>bugs</dc:creator>
      <dc:date>2011-03-11T23:01:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to write internal FLASH?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-write-internal-FLASH/m-p/190634#M2213</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It is possible to update SW in various manners and this is possibel with the Kinetis devices as with others, such as the M522XX Coldfire ones, which have similar FLASH.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The fact that there are 2 partitions in the larger chips means that it is possible to run code in one plane while executing Flash commands in the other, but this is not a main issue when uploading new code and it is also possible when using device with one Flash plane.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;See also: &lt;A href="http://www.utasker.com/docs/uTasker/BM-Booloader_for_M5223X.PDF" rel="nofollow" target="_self"&gt;http://www.utasker.com/docs/uTasker/BM-Booloader_for_M5223X.PDF&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Mar 2011 06:43:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-write-internal-FLASH/m-p/190634#M2213</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2011-03-13T06:43:13Z</dc:date>
    </item>
  </channel>
</rss>