<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Kinetis KL02 : Analog input absolute maximum rating</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL02-Analog-input-absolute-maximum-rating/m-p/396595#M21847</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are checking the device parameters for designing a custom board. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Background]&lt;BR /&gt;In the Data Sheet, Voltage and current operating ratings Tables,&lt;BR /&gt;it is described that&lt;BR /&gt;VDD [Digital supply vaoltage]&amp;nbsp; -0.3(Min.) --&amp;nbsp; 3.8(Max.)&lt;BR /&gt;VIO [IO pin input voltage]&amp;nbsp; -0.3(Min.)&amp;nbsp; --&amp;nbsp; VDD + 0.3(Max.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;BR /&gt;How much voltage is the Analog input absolute maximum rating ? &lt;BR /&gt;Is it identical to VIO voltage ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Koichi Sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Apr 2015 08:13:18 GMT</pubDate>
    <dc:creator>koichisakagami</dc:creator>
    <dc:date>2015-04-10T08:13:18Z</dc:date>
    <item>
      <title>Kinetis KL02 : Analog input absolute maximum rating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL02-Analog-input-absolute-maximum-rating/m-p/396595#M21847</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are checking the device parameters for designing a custom board. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Background]&lt;BR /&gt;In the Data Sheet, Voltage and current operating ratings Tables,&lt;BR /&gt;it is described that&lt;BR /&gt;VDD [Digital supply vaoltage]&amp;nbsp; -0.3(Min.) --&amp;nbsp; 3.8(Max.)&lt;BR /&gt;VIO [IO pin input voltage]&amp;nbsp; -0.3(Min.)&amp;nbsp; --&amp;nbsp; VDD + 0.3(Max.)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[Question]&lt;BR /&gt;How much voltage is the Analog input absolute maximum rating ? &lt;BR /&gt;Is it identical to VIO voltage ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Koichi Sakagami&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Apr 2015 08:13:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL02-Analog-input-absolute-maximum-rating/m-p/396595#M21847</guid>
      <dc:creator>koichisakagami</dc:creator>
      <dc:date>2015-04-10T08:13:18Z</dc:date>
    </item>
    <item>
      <title>Re: Kinetis KL02 : Analog input absolute maximum rating</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL02-Analog-input-absolute-maximum-rating/m-p/396596#M21848</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Koichi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry for the late reply,&lt;/P&gt;&lt;P&gt;If you are using the analog pin in the ADC the input voltage should be between VREFL(-100mV - 100mV ) and VREFH (min 1.13v - max 3.6v), if you are using CMP or DAC the input voltage should be MIN VSS-0.3V -- MAX VDD (1.71V - 3.6V) &lt;/P&gt;&lt;P&gt;You can check more information about the Analog Input electrical specifications in section 3.6 of the datasheet&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;Regards!&lt;/P&gt;&lt;P&gt;Patricia&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Apr 2015 15:43:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Kinetis-KL02-Analog-input-absolute-maximum-rating/m-p/396596#M21848</guid>
      <dc:creator>PatriciaTeran</dc:creator>
      <dc:date>2015-04-21T15:43:30Z</dc:date>
    </item>
  </channel>
</rss>