<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックIEEE 1588 PTP on FRDM K64F</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/IEEE-1588-PTP-on-FRDM-K64F/m-p/395428#M21712</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with multiple camera system (computer vision), and I would like to use FRDM K64F to sync the CAN,GPS,IMU datas with the camera clocks via IEEE 1588 ptp ethernet protocol. Moreover I want to provide trigger for the cameras in every 40ms. Does anybody have experiencies to configure this protocol? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Oct 2015 12:58:30 GMT</pubDate>
    <dc:creator>rolandkohari</dc:creator>
    <dc:date>2015-10-14T12:58:30Z</dc:date>
    <item>
      <title>IEEE 1588 PTP on FRDM K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/IEEE-1588-PTP-on-FRDM-K64F/m-p/395428#M21712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with multiple camera system (computer vision), and I would like to use FRDM K64F to sync the CAN,GPS,IMU datas with the camera clocks via IEEE 1588 ptp ethernet protocol. Moreover I want to provide trigger for the cameras in every 40ms. Does anybody have experiencies to configure this protocol? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 12:58:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/IEEE-1588-PTP-on-FRDM-K64F/m-p/395428#M21712</guid>
      <dc:creator>rolandkohari</dc:creator>
      <dc:date>2015-10-14T12:58:30Z</dc:date>
    </item>
    <item>
      <title>Re: IEEE 1588 PTP on FRDM K64F</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/IEEE-1588-PTP-on-FRDM-K64F/m-p/395429#M21713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is an application note &lt;A href="http://cache.freescale.com/files/analog/doc/app_note/AN4332.pdf"&gt;AN4332&lt;/A&gt; about IEEE1588 PTP application with Kinetis K60 product.&lt;/P&gt;&lt;P&gt;Related software please check with our third partner &lt;A href="http://www.ixxat.com/"&gt;IXXAT&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Oct 2015 06:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/IEEE-1588-PTP-on-FRDM-K64F/m-p/395429#M21713</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-10-21T06:15:57Z</dc:date>
    </item>
  </channel>
</rss>