<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: OpenSDA bare metal bring up in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-bare-metal-bring-up/m-p/394805#M21656</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;yes, you can add a K20 to your design and then use it to debug the 'master' device. We did that with the TinyK20 (but kept it on a separate board), see &lt;A href="http://mcuoneclipse.com/category/boards/tinyk20/" title="http://mcuoneclipse.com/category/boards/tinyk20/"&gt;TinyK20 | MCU on Eclipse&lt;/A&gt;. See the links and material in that article series, and make sure you read "&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-100720"&gt;https://community.freescale.com/docs/DOC-100720&lt;/A&gt;​".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;Do the microcontroller come up with pre-installed initial bootloader.&lt;/P&gt;&lt;P&gt;No, the K20 will come as a blank device. You need a SWD debug cable (Segger J-Link, P&amp;amp;E Multilink or a FRDM board (see &lt;A href="http://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/" title="http://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/"&gt;Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards&lt;/A&gt;)) to program it with the initial bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 20 Sep 2015 05:58:51 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2015-09-20T05:58:51Z</dc:date>
    <item>
      <title>OpenSDA bare metal bring up</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-bare-metal-bring-up/m-p/394804#M21655</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Freescale guys&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is my very first post to this community and before posting to the community I want to tell the community a little bit more about myself.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually I am embedded hobbyist and love to play with various controllers. I have tried Atmel, TIs MSP430 and ST microcontroller and some 8051 variants. I do this by designing and developing my own custom boards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ok that's it about my self.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now the query is:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am pretty much excited about the Freescale microcontrollers and up to till now I am using the ST microelectronics controller (as mentioned above). They provide too much in less amount and also their development tools are affordable especially debugger ST-Link.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But now I also want to try freescale products and for that I wanted to create my own custom board. and what make me more eager about it is the fact its &lt;STRONG&gt;open debugger OpenSDA&lt;/STRONG&gt;. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It says that put the debugger files in the microcontroller folder when it appears in the bootloader mode. So what I want to know is that if I have K20 microcontroller and design its OpenSDA schematic from reference design , than would the microcontroller would be able to enter into the bootloader mode. Do the microcontroller come up with pre-installed initial bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If no than what will be the procedure for burning that primary bootloader to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with warm regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Piyush Pandey&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 Sep 2015 12:12:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-bare-metal-bring-up/m-p/394804#M21655</guid>
      <dc:creator>piyushpandey</dc:creator>
      <dc:date>2015-09-19T12:12:37Z</dc:date>
    </item>
    <item>
      <title>Re: OpenSDA bare metal bring up</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-bare-metal-bring-up/m-p/394805#M21656</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;yes, you can add a K20 to your design and then use it to debug the 'master' device. We did that with the TinyK20 (but kept it on a separate board), see &lt;A href="http://mcuoneclipse.com/category/boards/tinyk20/" title="http://mcuoneclipse.com/category/boards/tinyk20/"&gt;TinyK20 | MCU on Eclipse&lt;/A&gt;. See the links and material in that article series, and make sure you read "&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-100720"&gt;https://community.freescale.com/docs/DOC-100720&lt;/A&gt;​".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;Do the microcontroller come up with pre-installed initial bootloader.&lt;/P&gt;&lt;P&gt;No, the K20 will come as a blank device. You need a SWD debug cable (Segger J-Link, P&amp;amp;E Multilink or a FRDM board (see &lt;A href="http://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/" title="http://mcuoneclipse.com/2015/08/19/using-the-freescale-freedom-frdm-kl43z-to-debug-other-boards/"&gt;Using the Freescale Freedom (FRDM-KL43Z) to Debug other Boards&lt;/A&gt;)) to program it with the initial bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Sep 2015 05:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/OpenSDA-bare-metal-bring-up/m-p/394805#M21656</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2015-09-20T05:58:51Z</dc:date>
    </item>
  </channel>
</rss>