<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMKE06Z128VLH4 and open collector circuit</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE06Z128VLH4-and-open-collector-circuit/m-p/394014#M21583</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just want to confirm what I read in ref. manual. &lt;/P&gt;&lt;P&gt;Is that true that only PTA2 and PTA3 (on MKE06Z128VLH4) can be used for open collector circuit?&lt;/P&gt;&lt;P&gt;If so, is the following seq. enough for configuration of the input/output &lt;SPAN style="font-size: 13.3333330154419px;"&gt;for open collector circuit&lt;/SPAN&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14304238441395329" jivemacro_uid="_14304238441395329" modifiedtitle="true"&gt;
&lt;P&gt;GPIOA_PDDR |= ( GPIO_PDD_PIN_2 );&lt;/P&gt;
&lt;P&gt;GPIOA_PIDR &amp;amp;= ~( GPIO_PDD_PIN_2 );&lt;/P&gt;
&lt;P&gt;PORT_PUE0&amp;nbsp; |= ( GPIO_PDD_PIN_2 );&lt;/P&gt;
&lt;P&gt;/* Set initialization value to high*/&lt;/P&gt;
&lt;P&gt;GPIOA_PDOR |= ( &lt;SPAN style="color: rgba(0, 0, 0, 0); font-family: Consolas, 'Courier New', Courier, mono, serif; font-size: 12px;"&gt;GPIO_PDD_PIN_2&lt;/SPAN&gt; );&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any possibility go get interrupt when pin 2 is falling? Should I use KBI for that purpose, would it work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Apr 2015 19:58:47 GMT</pubDate>
    <dc:creator>yuriydovgalyuk</dc:creator>
    <dc:date>2015-04-30T19:58:47Z</dc:date>
    <item>
      <title>MKE06Z128VLH4 and open collector circuit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE06Z128VLH4-and-open-collector-circuit/m-p/394014#M21583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just want to confirm what I read in ref. manual. &lt;/P&gt;&lt;P&gt;Is that true that only PTA2 and PTA3 (on MKE06Z128VLH4) can be used for open collector circuit?&lt;/P&gt;&lt;P&gt;If so, is the following seq. enough for configuration of the input/output &lt;SPAN style="font-size: 13.3333330154419px;"&gt;for open collector circuit&lt;/SPAN&gt;:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro jive_macro_code _jivemacro_uid_14304238441395329" jivemacro_uid="_14304238441395329" modifiedtitle="true"&gt;
&lt;P&gt;GPIOA_PDDR |= ( GPIO_PDD_PIN_2 );&lt;/P&gt;
&lt;P&gt;GPIOA_PIDR &amp;amp;= ~( GPIO_PDD_PIN_2 );&lt;/P&gt;
&lt;P&gt;PORT_PUE0&amp;nbsp; |= ( GPIO_PDD_PIN_2 );&lt;/P&gt;
&lt;P&gt;/* Set initialization value to high*/&lt;/P&gt;
&lt;P&gt;GPIOA_PDOR |= ( &lt;SPAN style="color: rgba(0, 0, 0, 0); font-family: Consolas, 'Courier New', Courier, mono, serif; font-size: 12px;"&gt;GPIO_PDD_PIN_2&lt;/SPAN&gt; );&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any possibility go get interrupt when pin 2 is falling? Should I use KBI for that purpose, would it work?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Apr 2015 19:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE06Z128VLH4-and-open-collector-circuit/m-p/394014#M21583</guid>
      <dc:creator>yuriydovgalyuk</dc:creator>
      <dc:date>2015-04-30T19:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: MKE06Z128VLH4 and open collector circuit</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE06Z128VLH4-and-open-collector-circuit/m-p/394015#M21584</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yuriy Dovalyuk,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; PTA2 and PTA3 are true open-drain pin when operated as output, and the internal pullup has no effect.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; But if you use these pins as the IIC, the internal pullup device remains active when PTAPE2, PTAPE3 is set, it is automatically disabled to save power when output low.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; So, except I2C module pin, PTA2 and PTA3 need add external pull up when it is configured as output.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; For KBI, because it is the input module, so you can use the internal pullup and can get the interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Jingjing&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2015 04:50:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MKE06Z128VLH4-and-open-collector-circuit/m-p/394015#M21584</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-05-04T04:50:54Z</dc:date>
    </item>
  </channel>
</rss>