<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: K60 interface with a parallel nor flash</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-interface-with-a-parallel-nor-flash/m-p/393855#M21578</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is our case. We have pins only for multiplexed mode. We know some flash memory as the MT28GU01GAAA2EGC0SIT with A/D MUX but it needs 1.7V-2V supply.&lt;/P&gt;&lt;P&gt;We will check if it is possible reduce the VDD from 3.3V to 2V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Jul 2015 14:46:20 GMT</pubDate>
    <dc:creator>javiervicandi</dc:creator>
    <dc:date>2015-07-09T14:46:20Z</dc:date>
    <item>
      <title>K60 interface with a parallel nor flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-interface-with-a-parallel-nor-flash/m-p/393853#M21576</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN class="hps"&gt;We need to use&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a parallel NOR&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;flash&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;memory&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;with&lt;/SPAN&gt; the &lt;SPAN class="hps"&gt;K60&lt;/SPAN&gt;. &lt;SPAN class="hps"&gt;We have not found&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;a memory with&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;multiplexed&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;address&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;and&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;data (&lt;/SPAN&gt;&lt;SPAN class="hps"&gt;size of 512Mb or&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;1Gb) to&lt;/SPAN&gt;&lt;SPAN class="hps"&gt;&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;connect&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;directly to&lt;/SPAN&gt; &lt;SPAN class="hps"&gt;FlexBus&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;A solution without external latches or changing to serial interface?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="en"&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 17:04:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-interface-with-a-parallel-nor-flash/m-p/393853#M21576</guid>
      <dc:creator>javiervicandi</dc:creator>
      <dc:date>2015-07-08T17:04:22Z</dc:date>
    </item>
    <item>
      <title>Re: K60 interface with a parallel nor flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-interface-with-a-parallel-nor-flash/m-p/393854#M21577</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;K60 Flexbus module provides non-multiplexed address and data busses connection, which based on customer K60 pin resource.&lt;/P&gt;&lt;P&gt;If K60 could not provides enough non-multiplexed address pin resource, it need to use the address latches.&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2015 03:05:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-interface-with-a-parallel-nor-flash/m-p/393854#M21577</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-07-09T03:05:23Z</dc:date>
    </item>
    <item>
      <title>Re: K60 interface with a parallel nor flash</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-interface-with-a-parallel-nor-flash/m-p/393855#M21578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is our case. We have pins only for multiplexed mode. We know some flash memory as the MT28GU01GAAA2EGC0SIT with A/D MUX but it needs 1.7V-2V supply.&lt;/P&gt;&lt;P&gt;We will check if it is possible reduce the VDD from 3.3V to 2V.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2015 14:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/K60-interface-with-a-parallel-nor-flash/m-p/393855#M21578</guid>
      <dc:creator>javiervicandi</dc:creator>
      <dc:date>2015-07-09T14:46:20Z</dc:date>
    </item>
  </channel>
</rss>