<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FlexCan: individual masking does not work in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCan-individual-masking-does-not-work/m-p/393062#M21511</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use individual masking functionality of FlexCAN by setup a mask to received CAN Message.&lt;/P&gt;&lt;P&gt; My setup is the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- use MB1 as receive message box&lt;/P&gt;&lt;P&gt;- IDAM bit = Format A&lt;/P&gt;&lt;P&gt;- IRMQ bit = 1 (individual masking is enabled and FIFO is not used)&lt;/P&gt;&lt;P&gt;- RXIMR1 = 0x00000700 (I want to receive all IDs between 0x300 and 0x3FF)&lt;/P&gt;&lt;P&gt;- ID = 0x300 therfore in MB[1].ID it is 0xC000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I verified&amp;nbsp; that the RXIMR1 register is written correctly in FreezeMode&lt;/P&gt;&lt;P&gt;I also verified that MB[1].ID is also written correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why do I get all CAN ID´s with this Setup and the defined mask (0x700) has no effect ?&lt;/P&gt;&lt;P&gt;Is there any additional configuration which I missed ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Jochen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Jul 2015 07:02:05 GMT</pubDate>
    <dc:creator>kilobyte</dc:creator>
    <dc:date>2015-07-08T07:02:05Z</dc:date>
    <item>
      <title>FlexCan: individual masking does not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCan-individual-masking-does-not-work/m-p/393062#M21511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I want to use individual masking functionality of FlexCAN by setup a mask to received CAN Message.&lt;/P&gt;&lt;P&gt; My setup is the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- use MB1 as receive message box&lt;/P&gt;&lt;P&gt;- IDAM bit = Format A&lt;/P&gt;&lt;P&gt;- IRMQ bit = 1 (individual masking is enabled and FIFO is not used)&lt;/P&gt;&lt;P&gt;- RXIMR1 = 0x00000700 (I want to receive all IDs between 0x300 and 0x3FF)&lt;/P&gt;&lt;P&gt;- ID = 0x300 therfore in MB[1].ID it is 0xC000000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I verified&amp;nbsp; that the RXIMR1 register is written correctly in FreezeMode&lt;/P&gt;&lt;P&gt;I also verified that MB[1].ID is also written correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why do I get all CAN ID´s with this Setup and the defined mask (0x700) has no effect ?&lt;/P&gt;&lt;P&gt;Is there any additional configuration which I missed ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;Jochen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Jul 2015 07:02:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCan-individual-masking-does-not-work/m-p/393062#M21511</guid>
      <dc:creator>kilobyte</dc:creator>
      <dc:date>2015-07-08T07:02:05Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCan: individual masking does not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCan-individual-masking-does-not-work/m-p/393063#M21512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jochen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check below message buffer structure:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/52711i07286A85BCD6F230/image-size/large?v=v2&amp;amp;px=999" title="2015-07-09_12-29-35.png" alt="2015-07-09_12-29-35.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The standard frame ID is from bit 28 to bit 18.&lt;/P&gt;&lt;P&gt;So the RXIMR1 = 0x00000700 should change to RXIMR1 = 0x1C000000&lt;/P&gt;&lt;P&gt;Wish it helps.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Ma Hui&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2015 04:34:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCan-individual-masking-does-not-work/m-p/393063#M21512</guid>
      <dc:creator>Hui_Ma</dc:creator>
      <dc:date>2015-07-09T04:34:03Z</dc:date>
    </item>
    <item>
      <title>Re: FlexCan: individual masking does not work</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCan-individual-masking-does-not-work/m-p/393064#M21513</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ma Hui,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks a lot for your Support!&lt;/P&gt;&lt;P&gt;That was exactly the solution I needed.&lt;/P&gt;&lt;P&gt;Now it works perfect!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Jochen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jul 2015 07:58:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/FlexCan-individual-masking-does-not-work/m-p/393064#M21513</guid>
      <dc:creator>kilobyte</dc:creator>
      <dc:date>2015-07-09T07:58:58Z</dc:date>
    </item>
  </channel>
</rss>