<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: KL Wakeup from LLS via UART Edge?</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL-Wakeup-from-LLS-via-UART-Edge/m-p/393053#M21510</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Greatly appreciated.&lt;/P&gt;&lt;P&gt;Ciarán&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Sep 2015 12:57:54 GMT</pubDate>
    <dc:creator>CiaranMacA_hkc</dc:creator>
    <dc:date>2015-09-23T12:57:54Z</dc:date>
    <item>
      <title>KL Wakeup from LLS via UART Edge?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL-Wakeup-from-LLS-via-UART-Edge/m-p/393050#M21507</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested wakeup from VLPS via UART Rx Edge. Fine. Works well. I enabled the RXEDGIE and clear RXEDGEIF in the interrupt. Fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What about LLS? Will this work (using LLWU)?&amp;nbsp; (I know that LLS wakeup is possible via LLWU external pins. That's ok, the question is , on UART Rx?)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Ciarán Mac Aonghusa&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 11:23:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL-Wakeup-from-LLS-via-UART-Edge/m-p/393050#M21507</guid>
      <dc:creator>CiaranMacA_hkc</dc:creator>
      <dc:date>2015-09-18T11:23:54Z</dc:date>
    </item>
    <item>
      <title>Re: KL Wakeup from LLS via UART Edge?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL-Wakeup-from-LLS-via-UART-Edge/m-p/393051#M21508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See &lt;A href="https://community.nxp.com/message/421247"&gt;Using Kinetis Low Power Stop Modes with unrestricted UART operation - a report&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The UART edge interrupt is only possible from STOP based modes and not LLS.&lt;/P&gt;&lt;P&gt;If you need to wake from a LLS mode (much slower) you will need a LLWU input instead. You could do this by connecting the UART input together with a LLWU input (in parallel).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 12:47:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL-Wakeup-from-LLS-via-UART-Edge/m-p/393051#M21508</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-09-18T12:47:43Z</dc:date>
    </item>
    <item>
      <title>Re: KL Wakeup from LLS via UART Edge?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL-Wakeup-from-LLS-via-UART-Edge/m-p/393052#M21509</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ciaran Mac Aonghusa,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Just like Mark Butcher have said,&amp;nbsp; LLS can't use the LLWU wake up with UART Rx, because the wakeup sources for LLWU inputs don't have it.&lt;/P&gt;&lt;P&gt;You can find the wakeup source for LLWU inputs in the reference manual, chapter 3. Wakeup sources for LLWU inputs. if you need the UART Rx to wake up, just as Mark suggest, you can connect the RX pin to the LLWU input pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish it helps you!&lt;/P&gt;&lt;P&gt;If you still have question, please contact with me!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jingjing&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2015 05:04:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL-Wakeup-from-LLS-via-UART-Edge/m-p/393052#M21509</guid>
      <dc:creator>kerryzhou</dc:creator>
      <dc:date>2015-09-21T05:04:38Z</dc:date>
    </item>
    <item>
      <title>Re: KL Wakeup from LLS via UART Edge?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL-Wakeup-from-LLS-via-UART-Edge/m-p/393053#M21510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, Greatly appreciated.&lt;/P&gt;&lt;P&gt;Ciarán&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Sep 2015 12:57:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KL-Wakeup-from-LLS-via-UART-Edge/m-p/393053#M21510</guid>
      <dc:creator>CiaranMacA_hkc</dc:creator>
      <dc:date>2015-09-23T12:57:54Z</dc:date>
    </item>
  </channel>
</rss>