<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis Microcontrollers中的主题 Re: Use VOUT33 to power other devices</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-VOUT33-to-power-other-devices/m-p/392318#M21391</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hello Thiago,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Indeed, you can use the VOUT33 to power another devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Provided that you adhere to the USB VREG electrical specifications mentioned on the &lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/KL43P64M48SF6.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.freescale.com/files/32bit/doc/data_sheet/KL43P64M48SF6.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;KL43 datasheet&lt;/A&gt;​, there will be no problems with the LPO from the USB regulator. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case the maximum output current the LPO can provide is up to 120 mA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Please be aware that the external circuit is not demanding more than this current, 120 mA. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information will be useful for you.&lt;/P&gt;&lt;P&gt;Have a great day.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards, :smileyhappy:&lt;/P&gt;&lt;P&gt;David Diaz.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Jun 2015 21:56:13 GMT</pubDate>
    <dc:creator>david_diaz</dc:creator>
    <dc:date>2015-06-11T21:56:13Z</dc:date>
    <item>
      <title>Use VOUT33 to power other devices</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-VOUT33-to-power-other-devices/m-p/392317#M21390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I use the VOUT33 pin to power other devices? It seems that it is pretty stable under 120mA and my board should be using far less than that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I have a dual power source option (5V via USB/VREGIN, or 3.3V from elsewhere) but only one of then will remain active at a given time (user choice), can I connect the VOUT33 and the 3.3V straight to each other without damaging the MCU? Maybe adding a schottky between them? I am using a KL43 chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thx&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2015 20:37:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-VOUT33-to-power-other-devices/m-p/392317#M21390</guid>
      <dc:creator>thiagopalmieri</dc:creator>
      <dc:date>2015-06-11T20:37:20Z</dc:date>
    </item>
    <item>
      <title>Re: Use VOUT33 to power other devices</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-VOUT33-to-power-other-devices/m-p/392318#M21391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hello Thiago,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Indeed, you can use the VOUT33 to power another devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Provided that you adhere to the USB VREG electrical specifications mentioned on the &lt;A href="http://cache.freescale.com/files/32bit/doc/data_sheet/KL43P64M48SF6.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf" title="http://cache.freescale.com/files/32bit/doc/data_sheet/KL43P64M48SF6.pdf?fasp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf"&gt;KL43 datasheet&lt;/A&gt;​, there will be no problems with the LPO from the USB regulator. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In this case the maximum output current the LPO can provide is up to 120 mA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Please be aware that the external circuit is not demanding more than this current, 120 mA. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this information will be useful for you.&lt;/P&gt;&lt;P&gt;Have a great day.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards, :smileyhappy:&lt;/P&gt;&lt;P&gt;David Diaz.&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jun 2015 21:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/Use-VOUT33-to-power-other-devices/m-p/392318#M21391</guid>
      <dc:creator>david_diaz</dc:creator>
      <dc:date>2015-06-11T21:56:13Z</dc:date>
    </item>
  </channel>
</rss>