<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KBI SP register in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391151#M21307</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an interrupt responding on a KBI interrupt pin.&amp;nbsp; However, when I look at the KBI_SP register to indicate which pin caused the interrupt, all bits are always set.&amp;nbsp; This is true even afer I write to the KBI_SC RSTKBSP bit to clear it.&amp;nbsp; This a MKE06Z128VLH4. I have confirmed that the address is correct for&amp;nbsp; both the KBI0_SP and KBI1_SP registers, but they are all set and don't appear to change.&amp;nbsp; Am I missing something?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jan 2015 21:32:57 GMT</pubDate>
    <dc:creator>davidsherman</dc:creator>
    <dc:date>2015-01-07T21:32:57Z</dc:date>
    <item>
      <title>KBI SP register</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391151#M21307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have an interrupt responding on a KBI interrupt pin.&amp;nbsp; However, when I look at the KBI_SP register to indicate which pin caused the interrupt, all bits are always set.&amp;nbsp; This is true even afer I write to the KBI_SC RSTKBSP bit to clear it.&amp;nbsp; This a MKE06Z128VLH4. I have confirmed that the address is correct for&amp;nbsp; both the KBI0_SP and KBI1_SP registers, but they are all set and don't appear to change.&amp;nbsp; Am I missing something?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 21:32:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391151#M21307</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2015-01-07T21:32:57Z</dc:date>
    </item>
    <item>
      <title>Re: KBI SP register</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391152#M21308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You need to set the KBSPEN bit in KBIx_SC to configure the correct flag mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49011i814247280A025030/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;http://www.utasker.com/kinetis.html&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 22:19:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391152#M21308</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-01-07T22:19:59Z</dc:date>
    </item>
    <item>
      <title>Re: KBI SP register</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391153#M21309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently implemented a KBI module for KE02, KE04 and KE06 processors (there are two versions, whereby the KE06 has the more luxurious one).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The KBIs are simulated in the uTasker Kinetis simulator and allow individual user interrupts to be allocated to each of the pins.&lt;/P&gt;&lt;P&gt;I have a KE06 package including KBI operation at &lt;A href="http://www.utasker.com/kinetis/FRDM-KE06Z.html" title="http://www.utasker.com/kinetis/FRDM-KE06Z.html"&gt;http://www.utasker.com/kinetis/FRDM-KE06Z.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;but haven't yet written up a module analysis. There is however some reference (for the simpler one) at&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/465138"&gt;Re: Re: GPIO pin as interrupt source KEA-64&lt;/A&gt;&lt;/P&gt;&lt;P&gt;and some discussion of risk involved with individial interrupt assignement at&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/message/465329#465329" title="https://community.freescale.com/message/465329#465329"&gt;https://community.freescale.com/message/465329#465329&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.utasker.com/kinetis.html" title="http://www.utasker.com/kinetis.html"&gt;µTasker Kinetis support&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 23:12:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391153#M21309</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-01-07T23:12:59Z</dc:date>
    </item>
    <item>
      <title>Re: KBI SP register</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391154#M21310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ah, I feel sheepish.&amp;nbsp; That was the one thing I had overlooked in the documentation.&amp;nbsp; Thank you, Mark!&amp;nbsp; It's working now.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jan 2015 00:23:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391154#M21310</guid>
      <dc:creator>davidsherman</dc:creator>
      <dc:date>2015-01-08T00:23:23Z</dc:date>
    </item>
    <item>
      <title>Re: KBI SP register</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391155#M21311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;David&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is strange but I also missed it when I was developing and had the same issue the first time I tested.&lt;/P&gt;&lt;P&gt;Even after I had read all bit details, that one sort of blends into the white background of the user's manual, since it doesn't really make much sense as to what it does - initially...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jan 2015 13:45:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/KBI-SP-register/m-p/391155#M21311</guid>
      <dc:creator>mjbcswitzerland</dc:creator>
      <dc:date>2015-01-08T13:45:35Z</dc:date>
    </item>
  </channel>
</rss>