<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックMQX UART Write Lockup when using Flow Control</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-UART-Write-Lockup-when-using-Flow-Control/m-p/390865#M21284</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use a device that needs to allow us to disable/enable flow control on the uart on the fly.&amp;nbsp; This normally works fine, but on occasion, the device does not enable flow control and therefore sending data to the uart causes a lockup (stuck in the driver send routines).&amp;nbsp; We would like to wrap this in a timeout and we are wondering if there is a built-in way to do this using MQX.&amp;nbsp; Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 07 Jan 2015 18:49:55 GMT</pubDate>
    <dc:creator>jmag99</dc:creator>
    <dc:date>2015-01-07T18:49:55Z</dc:date>
    <item>
      <title>MQX UART Write Lockup when using Flow Control</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-UART-Write-Lockup-when-using-Flow-Control/m-p/390865#M21284</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We use a device that needs to allow us to disable/enable flow control on the uart on the fly.&amp;nbsp; This normally works fine, but on occasion, the device does not enable flow control and therefore sending data to the uart causes a lockup (stuck in the driver send routines).&amp;nbsp; We would like to wrap this in a timeout and we are wondering if there is a built-in way to do this using MQX.&amp;nbsp; Any ideas?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jan 2015 18:49:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-UART-Write-Lockup-when-using-Flow-Control/m-p/390865#M21284</guid>
      <dc:creator>jmag99</dc:creator>
      <dc:date>2015-01-07T18:49:55Z</dc:date>
    </item>
    <item>
      <title>Re: MQX UART Write Lockup when using Flow Control</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-UART-Write-Lockup-when-using-Flow-Control/m-p/390866#M21285</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm afraid the UART's hardware does not support flow control activation on the fly; every time the flow control is enabled/disabled, the Tx and Rx pins must be disabled and re-enabled or the module reset for the changes to have effect. This means any time you change the flow control you will lose the connection with the UART counterpart.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Jan 2015 19:18:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/MQX-UART-Write-Lockup-when-using-Flow-Control/m-p/390866#M21285</guid>
      <dc:creator>apanecatl</dc:creator>
      <dc:date>2015-01-08T19:18:00Z</dc:date>
    </item>
  </channel>
</rss>