<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックLLS sleep with MQXLite on KInetis</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLS-sleep-with-MQXLite-on-KInetis/m-p/390126#M21223</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using mkl26zvlh4 and MQXlite.&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;I am trying to put mkl26zvlh4 to sleep in the idle task.I have an external interrupt at pin PTC4 which is supposed to wake up the MCU from sleep. For this I have made these changes in the processor expert.(Attached files)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I checked the current consumed by the MCU, it was still the same as before (about 5 mA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also worked out LLS sleep snippet from the manual (&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf&lt;/A&gt; page no 26) with a bareboaord project, then I could drop the current consuption by 5mA, also changing clock mode to internal clock during sleep(hence turning off the PLL) also reduced the current consumption by 5mA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I use this code snippet in my idle task in MQXLite project, the MCU does not respond to an interrupt. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any setting I am missing? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if I need to share more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Kaustubh Kagalkar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Dec 2014 01:25:30 GMT</pubDate>
    <dc:creator>kaustubhkagalka</dc:creator>
    <dc:date>2014-12-04T01:25:30Z</dc:date>
    <item>
      <title>LLS sleep with MQXLite on KInetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLS-sleep-with-MQXLite-on-KInetis/m-p/390126#M21223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using mkl26zvlh4 and MQXlite.&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;I am trying to put mkl26zvlh4 to sleep in the idle task.I have an external interrupt at pin PTC4 which is supposed to wake up the MCU from sleep. For this I have made these changes in the processor expert.(Attached files)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I checked the current consumed by the MCU, it was still the same as before (about 5 mA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also worked out LLS sleep snippet from the manual (&lt;A href="http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf" title="http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN4503.pdf&lt;/A&gt; page no 26) with a bareboaord project, then I could drop the current consuption by 5mA, also changing clock mode to internal clock during sleep(hence turning off the PLL) also reduced the current consumption by 5mA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, when I use this code snippet in my idle task in MQXLite project, the MCU does not respond to an interrupt. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any setting I am missing? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if I need to share more details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Kaustubh Kagalkar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2014 01:25:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLS-sleep-with-MQXLite-on-KInetis/m-p/390126#M21223</guid>
      <dc:creator>kaustubhkagalka</dc:creator>
      <dc:date>2014-12-04T01:25:30Z</dc:date>
    </item>
    <item>
      <title>Re: LLS sleep with MQXLite on KInetis</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLS-sleep-with-MQXLite-on-KInetis/m-p/390127#M21224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Kaustubh &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Please also check the application note &lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4470.pdf"&gt;AN4470&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;Also there is a some samples code for the KL25 using MQXlite on the instalation folder of codewarrior&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;....\CW MCU v10.6\MCU\CodeWarrior_Examples\Processor_Expert\MQXLite\Kinetis\FRDM_KL25Z&lt;/P&gt;&lt;P&gt;I hope this will help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Dec 2014 17:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/LLS-sleep-with-MQXLite-on-KInetis/m-p/390127#M21224</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2014-12-10T17:03:04Z</dc:date>
    </item>
  </channel>
</rss>