<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Kinetis MicrocontrollersのトピックRe: SPI 1  K60 TOWER confusion</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-1-K60-TOWER-confusion/m-p/188797#M2115</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I send a service request and the reply was that there is an error in documentation so I my finding was correct&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Apr 2013 05:19:42 GMT</pubDate>
    <dc:creator>luke_8</dc:creator>
    <dc:date>2013-04-29T05:19:42Z</dc:date>
    <item>
      <title>SPI 1  K60 TOWER confusion</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-1-K60-TOWER-confusion/m-p/188795#M2113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am confused in documentation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1) In TWR-K60512 users manual there are SPI1 on B7 - B11 tower pins&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;B7 - SPI1_CLK &amp;nbsp; &amp;nbsp; usage PTE2&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;B8 - SPI1_CS1 &amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;B9 - SPI1_CS0 &amp;nbsp; &amp;nbsp;usage PTE4&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;B10 - SPI1_MOSI &amp;nbsp; usage PTE1&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;B11 - SPI1_MISO &amp;nbsp; usage PTE3&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;2) In K60 reference manual chapter 10.3.1 there is signal multiplexing and pin assignment&lt;/P&gt;&lt;P&gt;There are SPI signals described as SPI1_SIN, SPI1_SCK, SPI1_SOUT.&lt;/P&gt;&lt;P&gt;Why the different labeling of signals in documents for one device?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The last curious thing is that I found that the my software using SPI1 sends data on the B11 which is PTE3 &amp;nbsp;- MISO or SIN!!!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2011 22:36:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-1-K60-TOWER-confusion/m-p/188795#M2113</guid>
      <dc:creator>luke_8</dc:creator>
      <dc:date>2011-12-08T22:36:50Z</dc:date>
    </item>
    <item>
      <title>Re: SPI 1  K60 TOWER confusion</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-1-K60-TOWER-confusion/m-p/188796#M2114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI, Luke,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The Tower System tries to use generic signal names for the Elevator Connectors. &amp;nbsp;Sometimes these will not match up exactly with the signal names for a given MCU or MPU that is designed into a Tower System controller module. &amp;nbsp;That's what you are seeing here. &amp;nbsp;The Kinetis SPI module does not automatically swap the input and output data based on the mode of operation (master or slave). &amp;nbsp;The signal names used are "Serial In (SIN)" and "Serial Out (SOUT)". &amp;nbsp;On the TWR-K60N512, we set the Kinetis MCU up as the master and connection SIN to the generic MISO (master in, slave out) signal, and SOUT to the generic MOSI (master out, slave in) signal.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope that helps,&lt;/P&gt;&lt;P&gt;-mnorman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2011 02:08:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-1-K60-TOWER-confusion/m-p/188796#M2114</guid>
      <dc:creator>mnorman</dc:creator>
      <dc:date>2011-12-15T02:08:14Z</dc:date>
    </item>
    <item>
      <title>Re: SPI 1  K60 TOWER confusion</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-1-K60-TOWER-confusion/m-p/188797#M2115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I send a service request and the reply was that there is an error in documentation so I my finding was correct&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Apr 2013 05:19:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/SPI-1-K60-TOWER-confusion/m-p/188797#M2115</guid>
      <dc:creator>luke_8</dc:creator>
      <dc:date>2013-04-29T05:19:42Z</dc:date>
    </item>
  </channel>
</rss>