<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to Debug with timeline response using CW10.6 with PE Multilink? in Kinetis Microcontrollers</title>
    <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Debug-with-timeline-response-using-CW10-6-with-PE/m-p/389413#M21129</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response. My function is interrupt based and is being called in isr routine i.e in events.c. If I am not wrong than while collecting the trace information in debug mode, the execution is slow and thats why the interrupt is not getting triggered ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Amit Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Sep 2014 03:34:19 GMT</pubDate>
    <dc:creator>Amit_Kumar1</dc:creator>
    <dc:date>2014-09-03T03:34:19Z</dc:date>
    <item>
      <title>How to Debug with timeline response using CW10.6 with PE Multilink?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Debug-with-timeline-response-using-CW10-6-with-PE/m-p/389411#M21127</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I wanted to know how much time is being consumed by each function of my code. I have made multiple files (8-9) for different functions. My main function contains only initialization rest everything is interrupt based. But Some how I am not getting the desired speed which I wanted. So I tried debugging it along with the time line response. Here I am only getting the functions being called in the main function, that too not all the functions. How do I get time response of all the functions being called ? Below is the timeline diagram of my program. I want similar timeline for all the functions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44468i3B3B715813878132/image-size/large?v=v2&amp;amp;px=999" title="debug.jpg" alt="debug.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Amit Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Aug 2014 03:21:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Debug-with-timeline-response-using-CW10-6-with-PE/m-p/389411#M21127</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2014-08-29T03:21:44Z</dc:date>
    </item>
    <item>
      <title>Re: How to Debug with timeline response using CW10.6 with PE Multilink?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Debug-with-timeline-response-using-CW10-6-with-PE/m-p/389412#M21128</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Amit Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;if a function is not called in your application when executing, the time consume of this function will not shows there.&lt;/P&gt;&lt;P&gt;to measure the time consumed, I would suggest call all functions in main function. after you get result, then, you can comment out these calls.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Rick&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Sep 2014 02:11:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Debug-with-timeline-response-using-CW10-6-with-PE/m-p/389412#M21128</guid>
      <dc:creator>Rick_Li</dc:creator>
      <dc:date>2014-09-03T02:11:13Z</dc:date>
    </item>
    <item>
      <title>Re: How to Debug with timeline response using CW10.6 with PE Multilink?</title>
      <link>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Debug-with-timeline-response-using-CW10-6-with-PE/m-p/389413#M21129</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the response. My function is interrupt based and is being called in isr routine i.e in events.c. If I am not wrong than while collecting the trace information in debug mode, the execution is slow and thats why the interrupt is not getting triggered ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;Amit Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Sep 2014 03:34:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Kinetis-Microcontrollers/How-to-Debug-with-timeline-response-using-CW10-6-with-PE/m-p/389413#M21129</guid>
      <dc:creator>Amit_Kumar1</dc:creator>
      <dc:date>2014-09-03T03:34:19Z</dc:date>
    </item>
  </channel>
</rss>